Arduino Forum Arduino Uno + Raspberry Pi + workout stepper.
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
  • Replies 15 replies
  • Subscribers 402 subscribers
  • Views 1494 views
  • Users 0 members are here
  • raspberrypi
  • arduino
Related

Arduino Uno + Raspberry Pi + workout stepper.

dtsartsanis
dtsartsanis over 10 years ago

Hi everybody this is a very simple project i just finished.

 

For this project i used an Arduino UNO, a Raspberry PI model B, a couple of leds and a workout stepper. Usually workout steppers have small displays and you have to look down to see the progress of your workout. In my project i managed to remove the old display, connected to Arduino UNO as a simple switch. Then UNO is running the sketch through the Raspberry and using Pyserial, Bottle.py and Arduino-Serial-to-Browser so we can have our stepps to our browser.

 

Raspberry PI is using the latest raspbian image and after we fully update and upgrade it, we have to install the Arduino IDE. i preferred to install the latest one 1.6.0 which works fine.We dont have to install pyserial because it is already installed, but we have to install Bootle.py (see here Bottle: Python Web Framework — Bottle 0.13-dev documentation ) and Arduino-Serial-to-Browser from here https://github.com/whichlight/Arduino-Serial-to-Browser .

 

We start by uploading the sketch to UNO, then we open a terminal and we run the Arduino-Serial-to-Browser.py and finally we can open a browser and we type http:/127.0.0.1:8080.

 

The Arduino also have 5 leds. 4 for our step progress and one blinking for every two steps because the sketch counts 1 step for every 2 physical steps.in the delay time i noticed that if you set 500 ms then we have 1 step for every 1 physical step.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Attachments:
arduino_stepper_counter_leds.ino.zip
  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago in reply to clem57 +2
    Well according to his code the Green lights every 2 steps, the other 4 light up sequentially at 500, 1000, 1500, 2000 steps. They all cycle in order above 2100 steps.
  • gadget.iom
    gadget.iom over 10 years ago +1
    Nice work! You could simplify your setup and look at arduino-ethernet bridges and host the web page on the UNO.
  • clem57
    clem57 over 10 years ago +1
    dtsartsanis I like the way you used the Raspberry Pi with Arduino. Especially Arduino-Serial-to-Browser software gem. The combination of Arduino Uno with Raspberry Pi looks to be equivalent to Arduino…
Parents
  • dtsartsanis
    dtsartsanis over 10 years ago

    Just managed to embed a youtube video to the html file

     

    Open with a text editor the index.html file at the Arduino-Serial-to-Browser folder and at the top add the following lines

     

    <html>

    <body>

      <object data="http://www.youtube.com/embed/W7qWa52k-nE"-->you can add here the video of your preference.

      width="560" height="315"></object>

    </body>

    </html>

     

    Then run the program and you are ready.

     

    *i forgot to plug in the audio jack to the Raspberry Pi and you cant hear any sound, but it plays fine and also this is with a wifi connection which is also fine for the model B.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to dtsartsanis

    dtsartsanis

        Fantastic way to exercise and watch the Ben Heck show.image

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 10 years ago in reply to dtsartsanis

    dtsartsanis

        Fantastic way to exercise and watch the Ben Heck show.image

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dtsartsanis
    dtsartsanis over 10 years ago in reply to clem57

    You can also use the above project with the Raspberry Pi A or A+ but the content of the serial port will be displayed at the terminal and we can save them also to a text file. We know that the Raspberry Pi A/A+ have only 256 memory so it would be very difficult to use the browser.

     

    Start a new txt file and add the code from the attached file and then saved it as a python file with a .py extension.

    Load the sketch to Arduino, next open a terminal and cd to the folder that you have saved the above file. Run the file with sudo python and your .py file.

    Your steps then will be displayed to your terminal and at the same time a file will be created in the same folder with your .py file, called templog.txt with your steps.

     

    If you see the code there are the below lines

     

    port.setDTR(False)

    port.flushInput()

    port.setDTR(True)

     

    these are important and if you remove them you will see your content displayed with \r\n at the end.So these 3 lines actually "cleaning" the serial from these characters.

     

    In situation where u want to save data from arduino's serial port  in a pc u can still use a very handy program called Cooltherm and can be found here Roger Meier's Freeware

    But in situation like the Raspberry Pi where u cannot  run x86 programs the above way is a good solution.

    U can also use the above code to save data from a temperature sensor connected to a Raspberry Pi (you will have to remove first the 3 lines above) and then insert the data from the .txt file to a LibreOffice file.

    Attachments:
    serial_port_data_logging.zip