Arduino Forum Arduino Uno + Raspberry Pi + workout stepper.
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
  • Replies 15 replies
  • Subscribers 402 subscribers
  • Views 1492 views
  • Users 0 members are here
  • raspberrypi
  • arduino
Related

Arduino Uno + Raspberry Pi + workout stepper.

dtsartsanis
dtsartsanis over 10 years ago

Hi everybody this is a very simple project i just finished.

 

For this project i used an Arduino UNO, a Raspberry PI model B, a couple of leds and a workout stepper. Usually workout steppers have small displays and you have to look down to see the progress of your workout. In my project i managed to remove the old display, connected to Arduino UNO as a simple switch. Then UNO is running the sketch through the Raspberry and using Pyserial, Bottle.py and Arduino-Serial-to-Browser so we can have our stepps to our browser.

 

Raspberry PI is using the latest raspbian image and after we fully update and upgrade it, we have to install the Arduino IDE. i preferred to install the latest one 1.6.0 which works fine.We dont have to install pyserial because it is already installed, but we have to install Bootle.py (see here Bottle: Python Web Framework — Bottle 0.13-dev documentation ) and Arduino-Serial-to-Browser from here https://github.com/whichlight/Arduino-Serial-to-Browser .

 

We start by uploading the sketch to UNO, then we open a terminal and we run the Arduino-Serial-to-Browser.py and finally we can open a browser and we type http:/127.0.0.1:8080.

 

The Arduino also have 5 leds. 4 for our step progress and one blinking for every two steps because the sketch counts 1 step for every 2 physical steps.in the delay time i noticed that if you set 500 ms then we have 1 step for every 1 physical step.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Attachments:
arduino_stepper_counter_leds.ino.zip
  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago in reply to clem57 +2
    Well according to his code the Green lights every 2 steps, the other 4 light up sequentially at 500, 1000, 1500, 2000 steps. They all cycle in order above 2100 steps.
  • gadget.iom
    gadget.iom over 10 years ago +1
    Nice work! You could simplify your setup and look at arduino-ethernet bridges and host the web page on the UNO.
  • clem57
    clem57 over 10 years ago +1
    dtsartsanis I like the way you used the Raspberry Pi with Arduino. Especially Arduino-Serial-to-Browser software gem. The combination of Arduino Uno with Raspberry Pi looks to be equivalent to Arduino…
Parents
  • dtsartsanis
    dtsartsanis over 10 years ago

    This is how u connect the stepper to the Arduino and the led's connections.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to dtsartsanis

    What do all the LED's tell you?image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago in reply to clem57

    Well according to his code the Green lights every 2 steps, the other 4 light up sequentially at 500, 1000, 1500, 2000 steps. They all cycle in order above 2100 steps.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to gadget.iom

    Thanks Paul

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 10 years ago in reply to gadget.iom

    Thanks Paul