Arduino Forum Arduino or RaspBerry or other?
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
  • Replies 8 replies
  • Subscribers 394 subscribers
  • Views 514 views
  • Users 0 members are here
Related

Arduino or RaspBerry or other?

lokkytron
lokkytron over 10 years ago

I know this could be a stupid question, but you could figure out that I am very noob about both boards and I would wish get some advice.

 

I will tell you something about what i want to do. Thank you in advance for your time and your consideration.

 

I need make a tiny mechanism with two DC motors with variable velocity to move a small led-laser pointer. The light point must draw some lines on a wall.

Those lines will be drawn programming the variability of the velocity of mentioned motors.

 

Additional info: I do not need the movement be quick but I need it be accurate

 

As I said, I am just beginning with this activity. Please, you be kind with me if I'm writting stupid things

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago +1
    The beam will need to move relatively quickly in order for the laser to draw lines visible to the naked eye. The process is called POV. Most commercial laser projectors employ galvanometers for this task…
  • murraymr
    murraymr over 10 years ago +1
    I have read elsewhere that Arduino is a little more optimized for tasks like this, but I think either will work fine.
  • lokkytron
    lokkytron over 10 years ago in reply to murraymr +1
    Thank you Michael Murray
Parents
  • bobcroft
    bobcroft over 10 years ago

    lokkytron,  I think an Arduino is best suited to your application since what you require is 'control' rather than computational capability.  You could use stepper motors in micro stepping mode for your application.  The motors would cause the laser device to trace its beam across or up and down the wall.  There are special shields that fit onto the UNO to control stepper motors or you build your own circuit on strip board or a PCB.  There are a number of Arduino libraries for stepper motor control, Google 'Arduino Stepper motor library' and a good selection comes up.  You will probably need an external power supply to run the motors as the Arduino is limited to 40 mA on its pins with a total of 200 mA for the UNO board.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • lokkytron
    lokkytron over 10 years ago in reply to bobcroft

    thank you bobcroft for your response, it completely fits what I need to know

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kidiccurus
    kidiccurus over 10 years ago in reply to lokkytron

    You could also use servo motors. These can usually be driven directly from the pwm pins and a power supply. Ben heck built something like this in his "getting started with launchpad" episode, but used a different dev board. He used servos and it worked fine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kidiccurus
    kidiccurus over 10 years ago in reply to lokkytron

    You could also use servo motors. These can usually be driven directly from the pwm pins and a power supply. Ben heck built something like this in his "getting started with launchpad" episode, but used a different dev board. He used servos and it worked fine.