Arduino Forum A fast digital IO
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
  • Replies 6 replies
  • Subscribers 393 subscribers
  • Views 837 views
  • Users 0 members are here
  • performance
Related

A fast digital IO

Workshopshed
Workshopshed over 10 years ago

I've not had an issue with performance of the I/O but here's a technique for squeezing a little more speed out of the ports without having significant code changes.

 

http://www.codeproject.com/Articles/732646/Fast-digital-I-O-for-Arduino

  • Sign in to reply
  • Cancel

Top Replies

  • Workshopshed
    Workshopshed over 10 years ago in reply to clem57 +1
    I think I get what you mean. Being able to standardise code is important if you are working on lots of different platforms and changing "core" libraries does pass compatibility issues onto your responsibility…
Parents
  • clem57
    clem57 over 10 years ago

    This looks nice until you see things like recent changing from Raspberry Pi to a Pi 2 and the library breaks! Too many folks here would not know what to do, except for some of the hard core type. image I have not checked, but would guess the Arduino has ports mapped differently depending on the chips also.

    Pass,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to clem57

    Clem Martins wrote:

     

    This looks nice until you see things like recent changing from Raspberry Pi to a Pi 2 and the library breaks! Too many folks here would not know what to do, except for some of the hard core type.

    Raspbian moved the peripheral base address from 2000.0000 to 3F00.0000.  It's probably hard-coded to 2000.0000 in most libraries.

     

    Here's a discussion at RasPi Forum: http://www.raspberrypi.org/forums/viewtopic.php?f=33&t=98740

     

    The RasPi GPIO Wiki hasn't been updated with the new value.  For that matter, it hasn't been updated completely for RasPi A+/B+ and RasPi 2.  Sic semper wikis.  http://elinux.org/RPi_Low-level_peripherals

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 10 years ago in reply to clem57

    Clem Martins wrote:

     

    This looks nice until you see things like recent changing from Raspberry Pi to a Pi 2 and the library breaks! Too many folks here would not know what to do, except for some of the hard core type.

    Raspbian moved the peripheral base address from 2000.0000 to 3F00.0000.  It's probably hard-coded to 2000.0000 in most libraries.

     

    Here's a discussion at RasPi Forum: http://www.raspberrypi.org/forums/viewtopic.php?f=33&t=98740

     

    The RasPi GPIO Wiki hasn't been updated with the new value.  For that matter, it hasn't been updated completely for RasPi A+/B+ and RasPi 2.  Sic semper wikis.  http://elinux.org/RPi_Low-level_peripherals