Arduino Forum How to interrupt delay?
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
  • Replies 4 replies
  • Subscribers 403 subscribers
  • Views 3143 views
  • Users 0 members are here
  • delay
Related

How to interrupt delay?

Former Member
Former Member over 10 years ago

Hi, it's me again,

 

So want to press button to close relay and then it opens after fixed time or I press button again, whichever comes first.  I can do the time, but I can't figure how to interrupt or halt the delay prematurely with a second button press.

 

I have tried replacing

 

int stayON = 10000;

delay(stayON);

 

with

 

int stayON = 100;

int var = 0;

            while(var < 100 && stateButton == LOW)

              {

                {

                delay(stayON);

                }

                var++;

              }

 

trying to break delay down into smaller increments and make it so if I press button then the while stops.  It works fine if I don't have any stateButton evaluations, but as soon as I add the button eval it just blinks when I press button but relay doesn't ever close.  I have tried a bazillion different ways of doing this with no luck and it's the only concept I have found, that I understand anyway.

 

Any help would be appreciated, thank you!

 

Full unmodified code below:

int pinButton = 10;
int Relay = 11;
int stateRelay = LOW;
int stateButton;
int previous = LOW;
long time = 0;
long debounce = 500;
int stayON = 10000;
void setup() {
pinMode(pinButton, INPUT);
pinMode(Relay, OUTPUT);
Serial.begin(9600);
}
void loop()
{
stateButton = digitalRead(pinButton);
if(stateButton == HIGH && previous == LOW && millis() - time > debounce)
{
  if(stateRelay == HIGH)
    {
      digitalWrite(Relay, LOW);
    } 
  else
    {
      digitalWrite(Relay, HIGH);
      Serial.print(1);
      delay(stayON);
      digitalWrite(Relay, LOW);
      Serial.print(2);
    }
time = millis();
}
previous == stateButton;
}
  • Sign in to reply
  • Cancel
  • Former Member
    Former Member over 10 years ago

    Ok I found the answer, go down to odometers post, it doesn't use the delay function and works perfectly.   Adafruit customer service forums • View topic - Countdown Timer Relay Sketch Help

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    The answer is not to use a DELAY() but a timer variable with a booleans to indicate the current state of the button and output set when you press the button, when you use a delay(), everything stops

     

    the following sudo code is an example, it could be optimized but I kept it simple for helping you to understand its operation, it also only has a very basic de-bounce but it should work once you code it into your target system language

     

    Hope it helps

     

     

    loop()

    {

     

    boolean myButton = false

    boolean myOutput = false

    long myTimer = 0

     

    if button is pressed and myButton is false and myOutput=false then

    {

    set output on

    set myOutput = true

    set myTimer = now + time delay

    set myButton = true // <-- prevents the button press from being repeated once you have accepted the command

    }

     

    if button is pressed and myButton is false and myOutput= true then // now checking if the button is pressed again and the output is on, therefore turn it off

    {

    set output off

    set myOutput = false

    set myButton = true

    }


    if myTimer < now then // timer has expired so turn off the output

    {

    set output off

    set myOutput = false

    // note this does not touch the button variable, this way if you hold the button for a long period the output will still turn off after the time period

    }


    if button is not pressed

    {

    set myButton = false // allow the button to be detected again

    }

     

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to Former Member

    check out the IMO porrly worded "BlinkWithoutDelay" in the examples in Arduino IDE.

     

    As peter said don't use Delay().

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to mcb1

    Yes, good point mcb1, that is a good example to refer to