Arduino Forum Arduino or Raspberry Pi?
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
  • Replies 2 replies
  • Subscribers 391 subscribers
  • Views 219 views
  • Users 0 members are here
Related

Arduino or Raspberry Pi?

couchie
couchie over 10 years ago

My appologies ahead of time for this not being an Arduino specific question, but I'm hoping those who are much smarter in these two areas and point me in the right direction....

 

A short(?) description of my project.....

 

Basicly three locations within a  building. Three RFID readers. Person one goes to room one, swipes RFID. RFID tag info is passed to a server and the data (tag ID, time/date) is written to a SQL DB. A LED strip over the door turns red.

 

Person one then goes to room 2 and the cycle repeats itself.

 

Now, person 2 goes to room 1, swipes his RFID and his info is logged back on the server. Now, when person one swiped, a LED strip on the outside of the door displays blue.

 

Pretty simple in theory and maybe I am over thinking this, but looking for a nudge in the right direction. Which would be more appropriate for this application? The Arduino or the Raspberry pi?

 

In my VERY limited experience, I'm thinking the Raspberry simply for the networking and USB functionality.

 

Looking forward to the input.

  • Sign in to reply
  • Cancel

Top Replies

  • lokkytron
    lokkytron over 10 years ago +1
    Hi Bob Couchman It sounds like an app that I made the last year with estimote and android. I mean you can achieve that without Arduino or RaspberryPi But if you need to make it with one or another. Though…
  • Anonymous-330417
    Anonymous-330417 over 10 years ago +1
    Both together would be kinda better as u can host the database on your RPi.. and do the I/O with arduinos.
  • lokkytron
    lokkytron over 10 years ago

    Hi Bob Couchman

     

    It sounds like an app that I made the last year with estimote and android.

    I mean you can achieve that without Arduino or RaspberryPi

     

    But if you need to make it with one or another.

    Though my experience with pi is null, I think the same way that you, with the pi it seems more easy to reach.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Anonymous-330417
    Anonymous-330417 over 10 years ago

    Both together would be kinda better as u can host the database on your RPi.. and do the I/O with arduinos.