Arduino Forum Using Arduino Uno to display a text string sent from a website?
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
  • Replies 3 replies
  • Subscribers 403 subscribers
  • Views 687 views
  • Users 0 members are here
  • wifi
  • webpage
  • arduino
Related

Using Arduino Uno to display a text string sent from a website?

Former Member
Former Member over 10 years ago

Hello there,

I have a quick question. Say I create a website and on it is a submit form with a text field. the user on the website enters the text and clicks submit. upon clicking submit; the text is send to an Arduino Uno, which is connected to a wifi shield and can be shown on either a serial monitor or lcd. How can this be achieved? In this scenario, is the Arduino acting as a client? server? does this webpage need to stored in the SD card of the wifi shield as well? please help. any advice would be greatly appreciated. thank you

cheers

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +1
    Ehsan kahn In the scenario you describe, the Uno is the web server and the page can be stored in memory as well as SD card. The server would be very small since the Uno has very little to work with. Why…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    Arduino is acting as a Server No the page does not need to be hosted on the Arduino Use of an LCD and Other things like using the Serial Port, with WIFI or Ethernet is all individually available but I…
Parents
  • lokkytron
    lokkytron over 10 years ago

    Hi Ehsan kahn

    I think THIS seems like you described

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • lokkytron
    lokkytron over 10 years ago

    Hi Ehsan kahn

    I think THIS seems like you described