Arduino
  • Products
  • More
Arduino
Arduino Forum New Arduino IDE
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 421 subscribers
  • Views 5142 views
  • Users 0 members are here
  • libraries
  • arduino
Related

New Arduino IDE

Workshopshed
Workshopshed over 11 years ago

There's been a few couple of upgrades to the Arudino IDE over the last month.

 

Arduino - Software

https://github.com/arduino/Arduino/blob/master/build/shared/revisions.txt

 

As I'm getting started with the Yun it's nice to see that some of the issues around that have been resolved but I think the feature I'm most interested in is the Library Manager, this should make working on different projects a whole lot easier.

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 11 years ago +4
    8 Minutes to download.... https://youtu.be/N1ug9-rhSs4?t=1m50s
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to neilk +3
    Neil, that's correct. Not only but I have explored a bit and see that the library manager is based on a JSON file including all the last updated library list organised by category. The json file is library_index…
  • WestfW
    WestfW over 11 years ago in reply to neilk +3
    > Microsoft standard software installation rules Sigh. I really hate the way that "Microsoft standard rules" scatter an application all over the disk :-(
Parents
  • Workshopshed
    Workshopshed over 11 years ago

    So far I've not found the new library manager to be of much help. I tried adding a library from zip and although that did create a library (in my user area) it did allow that library to reference other libraries which were in the program files folders. The net result was that it did not compile. I move the library over to the same folder structure as the others and it worked fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 11 years ago in reply to Workshopshed

    Workshopshed Hi Andy, my experience of installing libraries under Windows 7 is a bit happier:  under the 1.6.1 IDE,  I used the existing facility to install various libraries from their .zip files - they were installed in a folder called libraries, under the My Sketches Folder (which I keep elsewhere, and tell the IDE where to find it!!), not within the default Libraries folder.

     

    I subsequently used the provided uninstall program to remove 1.6.1 before installing 1.6.2. The libraries are still there; 1.6.2 can see them; I can load an example from one of them and it compiles happily.........I'm impressed.

     

    Separation of the downloaded IDE from "your own" stuff - sketches, external libraries etc seems to mark a big improvement.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to neilk

    I suppose that the fact that your libraries are already visible in 1.6.2 IDE is because the uninstaller only knows the files installed, so the settings files - generated locally by the first run and then modified by the preferences or other ways - are persistent from one setup to another.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • bobcroft
    bobcroft over 11 years ago in reply to neilk

    Neil,

              I do exactly as you do, keep my sketches in their own folder under the C:\ mysketches .  Libraries are a sub folder under  mysketches.  I put all my downloaded libraries in there and I have never had any problem with any IDE version right up to 1.6.3.  I cannot understand why the default path is something like C:\Windows\users\tomDickHarry\documents\Arduino, what a path!  I also put the manually installed Arduino IDE's directly under the C drive.  The .exe. installed ones go under programs(86).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bobcroft
    bobcroft over 11 years ago in reply to neilk

    Neil,

              I do exactly as you do, keep my sketches in their own folder under the C:\ mysketches .  Libraries are a sub folder under  mysketches.  I put all my downloaded libraries in there and I have never had any problem with any IDE version right up to 1.6.3.  I cannot understand why the default path is something like C:\Windows\users\tomDickHarry\documents\Arduino, what a path!  I also put the manually installed Arduino IDE's directly under the C drive.  The .exe. installed ones go under programs(86).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • neilk
    neilk over 11 years ago in reply to bobcroft

    bobcroft Hi Bob - in fact I go a little further further. All my Arduino "stuff", except for the IDE installation, Is held on a separate drive and in a top level folder that is synchronised by Dropbox. For me this means that I can work on both my desktop and my somewhat less powerful netbook, provided I install the IDE on both. It's very useful when I want to take Arduino on the road image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to neilk

    Nice. I make something like because all the essential things are on the Mac hard disks. When I need to work on Arduino under windows from one of the Virtualbox Win machines installed on the mac, I use the same location shared to the virtual machine. Then same on the local network when I use another computer, including a couple of Ubuntu devices.