Arduino Forum SdWebBrowse_CC3000_HTTPServer project
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
  • Replies 4 replies
  • Subscribers 401 subscribers
  • Views 610 views
  • Users 0 members are here
  • mega
  • ab9nq
  • logger
  • cc3000
  • sdwebbrowse
  • httpserver
  • data
  • arduino
Related

SdWebBrowse_CC3000_HTTPServer project

Former Member
Former Member over 10 years ago

Would like to share project...

 

Arduino Mega 2560; project with web server, file browser, and data logger.   Web server displays dynamic weather observations; plus there are two download links, one for current week’s weather observations, the other one is for previous weeks of weather observations.  Weather observation data is collected every 15 minutes for a 7 day duration; then file is appended with month and day form DS1307 Real Time Clock.  RTC 7th day of the week is used to trigger file rename.  Weather observation data is stored on a SD Card located on the “Adafruit CC3000 Shield,” which provides wireless connectivity to LAN. Sketch includes function to display Barometric pressure on a 16 X 2 LCD Display. 

 

Project can be found here: https://github.com/Tech500/SdWebBrowse-CC3000-HTTPServer

 

3:05 Minute, Video of project:  http://tinyurl.com/on5eaw2

 

William, AB9NQ

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 10 years ago

    Adding "Fritzing" breadboard to documentation for SdWebBrowse-CC3000-HTTPServer project:

                        image

    William

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ab9nq
    ab9nq over 9 years ago in reply to Former Member

    Project:  SdWebBrowse_CC3000_HTTPServer.ino  Data Logger and HTTP Web Server

    Latest update: 7/10/2016 @ 00:07 EST

     

    ~ 5 Minute "YouTube" video of project:  http://tinyurl.com/tech500-embedded

     

    Open Source project: https://github.com/Tech500/SdWebBrowse-CC3000-HTTPServer

     

    William

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ab9nq
    ab9nq over 9 years ago in reply to Former Member

    Project:  SdWebBrowse_CC3000_HTTPServer.ino  Data Logger and HTTP Web Server

    Latest update: 7/10/2016 @ 00:07 EST

     

    ~ 5 Minute "YouTube" video of project:  http://tinyurl.com/tech500-embedded

     

    Open Source project: https://github.com/Tech500/SdWebBrowse-CC3000-HTTPServer

     

    William