Arduino Forum Tre availability
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
  • Replies 4 replies
  • Subscribers 402 subscribers
  • Views 501 views
  • Users 0 members are here
  • arduino_tre
Related

Tre availability

markvenn
markvenn over 10 years ago

Has anyone heard any whispers about when the Tre will be available? I really want to get hold of one of these bits of kit. arduino.cc still says that it will be available soon, arduino.org does not mention it. (I assume this is due to the fact the board will be built in the US).

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +1
    In addition, the Arduino TRE is partially the result of a close collaboration between Arduino and the BeagleBoard.org foundation. These open hardware pioneers share a passion for expanding open source…
  • markvenn
    markvenn over 10 years ago in reply to clem57 +1
    That's the one! It looks like an arduino just dropped onto a huge shield But look at all those connections, X-Bee built in ! Really want to get one! the link talks about the board and give an expected…
  • cstanton
    cstanton over 10 years ago +1
    They're still working on it. Earlier this year they released another batch of developer editions. The IDE still has many bugs and when I have time I mess about with it: Hands on with the Arduino Tre :…
Parents
  • clem57
    clem57 over 10 years ago

    In addition, the Arduino TRE is partially the result of a close collaboration between Arduino and the BeagleBoard.org foundation. These open hardware pioneers share a passion for expanding open source development and making technology accessible for artists, designers and hobbyists. The TRE design builds upon the experience of both Arduino and BeagleBoard.org, combining the benefits of both community based boards.

    “By choosing TI’s Sitara AM335x processor to power the Arduino TRE, we’re enabling customers to leverage the capabilities of an exponentially faster processor running full Linux,” said Massimo Banzi, co-founder, Arduino. “Our customers now have a scalable portfolio at their fingertips, from the microcontroller-based Uno to the TRE Linux computer.”  http://makezine.com/2013/10/03/arduino-announces-two-new-linux-boards/

    image

     

    This?

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • markvenn
    markvenn over 10 years ago in reply to clem57

    That's the one! It looks like an arduino just dropped onto a huge shield But look at all those connections, X-Bee built in ! Really want to get one!

     

    the link talks about the board and give an expected release of

    They’re expecting to ship the Arduino TRE in Spring 2014

    So only a year late and still no  word.... image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • markvenn
    markvenn over 10 years ago in reply to clem57

    That's the one! It looks like an arduino just dropped onto a huge shield But look at all those connections, X-Bee built in ! Really want to get one!

     

    the link talks about the board and give an expected release of

    They’re expecting to ship the Arduino TRE in Spring 2014

    So only a year late and still no  word.... image