Arduino Forum Motor reverse safety
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
  • Replies 3 replies
  • Subscribers 391 subscribers
  • Views 288 views
  • Users 0 members are here
  • reverse
  • motor
  • arduino
  • safety
Related

Motor reverse safety

Former Member
Former Member over 10 years ago

I'm working on a dog door project that behaves similarly to a garage door. This is my first project with motors and I've hit a wall in my research. I want the door to be rugged so it would take considerable effort for other animals to get in but I don't want the door to injure the dogs if they try going through at the wrong time. How can I detect resistance in the doors movement so that I can reverse automatically? Currently working with a Titan 550 brush motor that I picked up at a hobby store.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +1
    Hi Joshua, As bobcroft says, it may be easier to find a motor with a gearbox, rather than try to build a gearbox. I think it will he hard to create something safe, unless you're quite experienced with…
Parents
  • shabaz
    shabaz over 10 years ago

    Hi Joshua,

     

    As bobcroft says, it may be easier to find a motor with a gearbox, rather than try to build a gearbox. I think it will he hard to create something safe, unless you're quite experienced with electronics and mechanics. I'd personally avoid such a project myself too, and just find conventional ways to let the dog in/out if possible.

    Also, it can happen that a motor driver turns faulty and just runs.. in which case reversing may not be possible if such a fault occurs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 10 years ago

    Hi Joshua,

     

    As bobcroft says, it may be easier to find a motor with a gearbox, rather than try to build a gearbox. I think it will he hard to create something safe, unless you're quite experienced with electronics and mechanics. I'd personally avoid such a project myself too, and just find conventional ways to let the dog in/out if possible.

    Also, it can happen that a motor driver turns faulty and just runs.. in which case reversing may not be possible if such a fault occurs.