Arduino Forum Temperature controlled relay (help needed for noobie)
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
  • Replies 17 replies
  • Subscribers 405 subscribers
  • Views 1113 views
  • Users 0 members are here
  • temperature
  • arduino
  • relay
Related

Temperature controlled relay (help needed for noobie)

Former Member
Former Member over 10 years ago

Hello, my name is Aisha this is my first post and I am excited to get into the community.


I live in a studio apartment with my wife. The entire apartment is on a 15amp breaker so we have to be careful about power use. We find if we run the A/C and cook something in the kitchen the fridge will kick on more often and trip our breaker. We have a blower to pull hot air out of the kitchen and I would like to use an arduino to turn it off and on based on the temperature.


I have:

 

an arduino uno

a tmp36 temperature sensor

a 5v arduino relay module

a breadboard and leads

 

I want to do this not only the right way and the best way with what I have available. I have used the arduino to switch the relay using the blinking LED code from a kit I got. I have wired up the sensor and read readings off of it.

 

 

The tutorials I find online say I should connect it to 3.3v and also AREF to 3.3v when I do this I don't get 3.3v in my serial monitor like the tutorials say but 1.5 (average). I am left lost as no tutorials show how to do this without an LCD screen and with a relay module. I don't need to monitor the temperature after I have it set properly once so an LCD is unnecessary (though I would not mind being able to add on in the future.)

 

I plan to put the sensor on a cable, are there limits to how long a cable can be for this sensor? I was planning on using cat5 cable.

 

So far all of my experiments with arduino involve copy pasting code and maybe modifying a couple lines that are clearly labeled or that a tutorial has told me to edit. I have 0% skills and about as much understanding and confidence in coding anything let alone a micro controller.

 

I have seen people adding things like data logging to increase accuracy of readings and delays to keep the switch from tripping like crazy but again I'm still struggling with the hardware and code is not at my level yet.

 

Hopefully there are people who can help me out. I know this is super easy for anyone who knows how to use and code arduino, I just need some help getting my first project finished.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +4
    aishalove First off, programming is not "super easy" as you say. I have done this most of my life and the biggest headache is to fix broken code. Even I break and fix my own code. I suggest read some about…
  • neilk
    neilk over 10 years ago +3
    aishalove Clem and Enrico have given you sound advice . For what it's worth, I have 2 basic rules when I am developing a project: Start small with something that should work - an example from the Arduino…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    What had not been said yet is the issue of driving mains with an arduino relay board. They are not all created to handle mains . Even if the physical elay is capable. The board may not be and mistakes…
Parents
  • clem57
    clem57 over 10 years ago

    aishalove

    First off, programming is not "super easy" as you say. I have done this most of my life and the biggest headache is to fix broken code. Even I break and fix my own code. I suggest read some about coding logic and play to learn.Start off with a blinking LED for example.

    Next make it blink slower the first time and faster the second time, Make it blink 4 times fast and 2 times slow. Each exercise build your knowledge and confidence, If it does not work the way you think you planned, run through the code with pencil and paper to determine why.

    Next add a button or two to start or change the blinking. You may think this is silly, but try to follow and you will learn more than you expect.

    Clem

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 10 years ago

    aishalove

    First off, programming is not "super easy" as you say. I have done this most of my life and the biggest headache is to fix broken code. Even I break and fix my own code. I suggest read some about coding logic and play to learn.Start off with a blinking LED for example.

    Next make it blink slower the first time and faster the second time, Make it blink 4 times fast and 2 times slow. Each exercise build your knowledge and confidence, If it does not work the way you think you planned, run through the code with pencil and paper to determine why.

    Next add a button or two to start or change the blinking. You may think this is silly, but try to follow and you will learn more than you expect.

    Clem

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to clem57

    Perfectly agreeing image