Arduino Forum Temperature controlled relay (help needed for noobie)
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
  • Replies 17 replies
  • Subscribers 394 subscribers
  • Views 973 views
  • Users 0 members are here
  • temperature
  • arduino
  • relay
Related

Temperature controlled relay (help needed for noobie)

Former Member
Former Member over 10 years ago

Hello, my name is Aisha this is my first post and I am excited to get into the community.


I live in a studio apartment with my wife. The entire apartment is on a 15amp breaker so we have to be careful about power use. We find if we run the A/C and cook something in the kitchen the fridge will kick on more often and trip our breaker. We have a blower to pull hot air out of the kitchen and I would like to use an arduino to turn it off and on based on the temperature.


I have:

 

an arduino uno

a tmp36 temperature sensor

a 5v arduino relay module

a breadboard and leads

 

I want to do this not only the right way and the best way with what I have available. I have used the arduino to switch the relay using the blinking LED code from a kit I got. I have wired up the sensor and read readings off of it.

 

 

The tutorials I find online say I should connect it to 3.3v and also AREF to 3.3v when I do this I don't get 3.3v in my serial monitor like the tutorials say but 1.5 (average). I am left lost as no tutorials show how to do this without an LCD screen and with a relay module. I don't need to monitor the temperature after I have it set properly once so an LCD is unnecessary (though I would not mind being able to add on in the future.)

 

I plan to put the sensor on a cable, are there limits to how long a cable can be for this sensor? I was planning on using cat5 cable.

 

So far all of my experiments with arduino involve copy pasting code and maybe modifying a couple lines that are clearly labeled or that a tutorial has told me to edit. I have 0% skills and about as much understanding and confidence in coding anything let alone a micro controller.

 

I have seen people adding things like data logging to increase accuracy of readings and delays to keep the switch from tripping like crazy but again I'm still struggling with the hardware and code is not at my level yet.

 

Hopefully there are people who can help me out. I know this is super easy for anyone who knows how to use and code arduino, I just need some help getting my first project finished.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +4
    aishalove First off, programming is not "super easy" as you say. I have done this most of my life and the biggest headache is to fix broken code. Even I break and fix my own code. I suggest read some about…
  • neilk
    neilk over 10 years ago +3
    aishalove Clem and Enrico have given you sound advice . For what it's worth, I have 2 basic rules when I am developing a project: Start small with something that should work - an example from the Arduino…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    What had not been said yet is the issue of driving mains with an arduino relay board. They are not all created to handle mains . Even if the physical elay is capable. The board may not be and mistakes…
  • Former Member
    Former Member over 10 years ago

    I have a major breakthrough! I found a code example for switching an LED using a temp sensor. I successfully used it to toggle my relay!

     

    This is the example I used

     

    http://www.dave-auld.net/index.php?option=com_content&view=article&id=89:arduino-analogue-in-temperature&catid=53:arduino-input-output-basics&Itemid=107

     

    All I did was change the digital pin 7 to the sens on my relay and bingo it works! The only issue I have is when I change the trigger temp it won't upload unless I try over and over until it works as a fluke (recompiling doesn't seem to help) or re paste the code, recompile and then upload and often that still gives errors.

     

    The error I am getting is "Error: process returned not zero code: 1"

     

    I have yet to get on my pc to try uploading using the official IDE, I use a smart phone as a programmer because I don't have room for my pc at my desk.

     

    Here is my proof of concept on a breadboard (Right now I am lighting an LED using the relay, after working out my upload error I will move on to a small AC indicator light.

     

    https://www.dropbox.com/s/ocui6plj2dlwzza/20150518_135910.jpg?dl=0

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago

    More progress, I have a full working proof of concept now. I also figured out it was my phone causing my upload issues.

     

    https://www.dropbox.com/s/eqliwhrznwdwkbc/20150518_142405.jpg?dl=0

     

    Now all I need to do is put it in a case. I would prefer to not have to solder anything to the arduinop so I can use it in the future for another project, but I don't trust the leads I have to stay put. Any suggestions?

     

    I figure a proto shield or something similar would be a good idea but I would prefer to use what I have on hand.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago

    Ok so my project is finished.

     

    https://www.dropbox.com/sh/0e0ugxri7f4yvk6/AAAR86WbKYJV2s8EvhuOiOxza?dl=0


    I know it looks sloppy, but it works great and it's my first successful build. ^____^

     

    All I need to do now is calibrate it for my kitchen.

     

    I truly want to thank everyone who provided advice and feedback, and I want to say I appreciate the notes about safety as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to Former Member

    Aisha

    It is great you have completed a project ...BUT ... electrical safety is something not to be ignored.

     

    Hot Glue to hold the mains cables and a cardboard box combined with mains voltage is not safe.

     

    FOR ANYONE ELSE CONSIDERING COPYING THIS PLEASE USE SAFE MAINS PRACTICES.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to mcb1

    I am unsure what is dangerous about using the hot glue. I soldered everything. The glue is mostly to physically keep the power connector in the box.

     

    My fan doesn't draw that much power so I don't see heat becoming an issue with the electrical connections.

     

    I don't want to sound argumentative but I simply don't understand the issue with this project and the hot glue.

     

    I would be worried about the box and and  insulation on the wires if it was likely to get that hot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to Former Member

    I am unsure what is dangerous

    That is why we try to provide education about the dangers.

     

    Relying on hot glue to stop the cable from being pulled and exposing the wires is one issue.

    The cardboard box is not a suitable insulator if it becomes damp, and will in fact conduct, and since it is not earthed, then it potentially become live.

    The fact that the cardboard box privides no ability to earth and has no strength is another.

     

    While you might be careful and treat it with care, what about a small child, or someone tripping on the wire.

    How would you feel if the item you created was the cause of injury to someone else?

     

     

    If you type Unsafe Mains into the site search, you will find numerous posts where we have raised similar issues.

    image

     

    So please don't feel I am targetting you personally,  .... just the practice.

     

    If you want advise on how to minimise these risks, then we are more than happy to assist, but you should open it a as new discussion.

     

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to mcb1

    I am absolutely with Mark on this one. While you get top marks with project progression, it would be a Zero for the enclosure and safety.

     

    The glue may hold the cable but the cardboard will not hold the glue or any of the other parts in the "Shoe Box" style enclosure. one drop and everything will go flying

     

    You can get some very good and reasonable priced enclosure from most local hardware store (Look at my Safety Box as an example Safety Outlet for the Home Bench or Lab). Actually this video was all about safe practices in the lab.

     

    And you have stated this project is going into a kitchen, this is a place prone to moisture or worse so the requirements are way higher

     

    Please fix the enclosure, board mounting and strain relief, then we should be much happier image

     

    Oh and as Mark stated, this is not personal, we will comment on any project showing bad (Unsafe) Practices. This is a family show after all.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<