Arduino Forum Shuttle/Jog HID
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
  • Replies 0 replies
  • Subscribers 389 subscribers
  • Views 125 views
  • Users 0 members are here
  • question
Related

Shuttle/Jog HID

Former Member
Former Member over 10 years ago

Hello,

I got a old Sony RM-450 editing control and moding it to USB,

I wired the keys to a old keyboard and use Quick Macros to remap the keys, Works good.

I need help with the two Shuttle/Jug controls. I’m going use a arduino uno  but never used one before.

 

I traced out the circuit

The Optical Sensors are sharp GP1L52

J2 is a NEC uPC339 low power quad comparator pin 13 is pin 1 on the IC

J1 is the wires off board.

 

Q2 and Q4 are for the indexing wheel

When in shuttle mode the wheel turns shy of 180 degrees each way and spring returns, A finger goes in front Q3 in the home position

When in Jog mode a finger goes in front Q1 and the wheel can spin freely, Q3 stays blocked    

 

So I think the program should go something like this.

When Q1 in blocked go into jog mode

When Q2 is blocked and Q4 is clear, send keyboard simulator “ctrl, left arrow”

When Q4 is blocked and Q2 is clear, send keyboard simulator “ctrl, right arrow”

 

When Q1 in clear go into shuttle mode

When Q2 is blocked and Q4 is clear, send keyboard simulator “left arrow”,  loop a percent faster each cycle

When Q4 is blocked and Q2 is clear, send keyboard simulator “left arrow”, loop a percent slower each cycle

When Q3 is blocked stop/reset

 

When Q4 is blocked and Q2 is clear, send keyboard simulator “right arrow”, loop a percent faster each cycle

When Q2 is blocked and Q4 is clear, send keyboard simulator “right arrow”,  loop a percent slower each cycle

When Q3 is blocked stop/reset

 

I don't know

Any help would be greatly appreciated.

 

Best of days

Andrew Popoff

Attachments: