Arduino
  • Products
  • More
Arduino
Arduino Forum Blank Arduino Sketch Uses 450 Bytes of Program Storage Space and has 9 Bytes of Global Variable?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 421 subscribers
  • Views 4546 views
  • Users 0 members are here
  • program
  • storage
  • arduino
  • variables
Related

Blank Arduino Sketch Uses 450 Bytes of Program Storage Space and has 9 Bytes of Global Variable?

oogutierrez
oogutierrez over 11 years ago

Does anyone know why a blank Arduino Sketch Uses 450 Bytes of Program Storage Space and has 9 Bytes of Global Variable? Why?

How does this compare with other AVR compilers?

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • fvan
    fvan over 11 years ago +2
    There seems to be a detailed explanation here: Analysis of an Empty Arduino Sketch Frederick
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to oogutierrez +2
    If you use the AVR Studio (I am using version 6) you see that the setup() and loop() functions can be defined to obtain the behaviour of the sketch IDE. Just the fact that you declare these functions mean…
  • mcb1
    mcb1 over 11 years ago in reply to clem57 +1
    Just to add. While the code shows nothing, there are various libraries and other settings that get compiled and sent to the board. Often its not the size of the sketch, but the libraries that take up most…
Parents
  • dmaruska
    dmaruska over 11 years ago

    Hi all, I'm new to Arduino and C programming.  I noticed the version of the compiler being used.  Its V1.7.3.  The latest release is V1.6.4  Is it something to do with the version?  Also, is this just to insure that you use as little of the Arduino memory for your programs.  Thanks.

     

    Regards,

     

    Dave M.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dmaruska
    dmaruska over 11 years ago

    Hi all, I'm new to Arduino and C programming.  I noticed the version of the compiler being used.  Its V1.7.3.  The latest release is V1.6.4  Is it something to do with the version?  Also, is this just to insure that you use as little of the Arduino memory for your programs.  Thanks.

     

    Regards,

     

    Dave M.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • oogutierrez
    oogutierrez over 11 years ago in reply to dmaruska

    dmaruska, yes this is to compare and see which IDE would produce less memory usage.

    i understand that Arduino may be quite easier to use but I am interested to see if other IDEs will get us better mileage and hopefully try to learn to code with the best one.

    since Arduino is simply a program and I believe you can program it with other AVR programming capable IDEs.

     

    i have been playing around with the Arduino IDE and sometimes find it uses so much memory that I sometimes run low in memory and get a 'low memory' warning of which I cannot explain and trying to understand why myself. also, be careful with using  so much 'serial.print()' in your code as it is a memory hog.