Arduino Forum Need help. How to wire up the Sainsmart 2.4" TFT LCD to Arduino Uno?
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
  • Replies 3 replies
  • Subscribers 402 subscribers
  • Views 720 views
  • Users 0 members are here
  • lcd
  • tft
  • SainSmart
  • arduino
Related

Need help. How to wire up the Sainsmart 2.4" TFT LCD to Arduino Uno?

oogutierrez
oogutierrez over 10 years ago

imageimage

I recently bought the TFT LCD shown in the image but unfortunately I cannot find a manual how to wire this up to Arduino Uno.

Can anyone help me get the resources I need to get this up and running?

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    If you want to understand how to use this on many different controllers then may I suggest you start with the controller chip, the pinout of the chip should align with the pins of the card you have (Same…
  • gadget.iom
    gadget.iom over 10 years ago +1
    There is a shield adaptor available for the UNO that may be helpful for you
  • gadget.iom
    gadget.iom over 10 years ago

    There is a shield adaptor available for the UNO that may be helpful for you

    04_17_14.jpg

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • oogutierrez
    oogutierrez over 10 years ago in reply to gadget.iom

    Thanks Paul. I may consider that adapter.

    However, I would like to know how to wire them so I can fully understand how it operates especially if I try other microcontrollers. I have Arduino, PIC and the TI launchpad. I just would like to start developing it on Arduino and port it to the other micros.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    If you want to understand how to use this on many different controllers then may I suggest you start with the controller chip, the pinout of the chip should align with the pins of the card you have (Same descriptions) and then you can se exactly how to use it

     

    https://www.sparkfun.com/datasheets/LCD/ILI9325.pdf

    or

    http://www.adafruit.com/datasheets/ILI9325.pdf

     

    AdaFruit also has an extensive graphics library etc for it. See here for details:2.8 18-bit color TFT LCD with touchscreen breakout board [ILI9325] ID: 335 - $40.00 : Adafruit Industries, Unique & fun …

    • Cancel
    • Vote Up +2 Vote Down