Arduino Forum Accelerometer Automated Locking system
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
  • Replies 42 replies
  • Subscribers 393 subscribers
  • Views 3632 views
  • Users 0 members are here
Related

Accelerometer Automated Locking system

Former Member
Former Member over 10 years ago

Hello,

 

I am Yuvish Chintaram from Mauritius Island.

 

Recently, I have applied to a university and my acceptance would be considered on a project that would help to contribute to my society.

My other friends are planting mangroves to help protect the marine ecosystem but I am more interested in science  and think to have find an interesting project.

 

A few months ago, an accident occured to a student that fell from a moving bus.(I have send you the link below.)

Surprisingly, two more people fell from a moving bus from the back emergency door after the earlier incident.

A solution was found by the Government that all bus should have an alarm and  that when the door opens an alarm will ring. But this does not solve the problem!

 

Hence, my idea was to incorporate a locking system that is fully autonomous. The system should lock the door while the bus is moving but unlock itself when the bus stops at a bustop.

I was thinking of using an accelerometer that will detect the acceleration of the bus that will relay to a circuit such that at a minimum value the latter will send a signal that will automatically lock or unlock the system.

eg. If(X>200)

      eletric lock is lock  

      else if (X<200)
       electric.lock is unlock

 

I am here to ask you if you could give me some advice and also if my current solution will work.

I would also be pleased to know your ideas about my project.( How would you answer it, etc..)

I would really appreciate if you could reply me as soon as possible.

 

http://news.islandcrisis.net/2015/03/17-year-old-student-keshnee-purmasing-died-after-falling-from-school-bus/

 

Regards

Yuvish Chintaram

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    Given that once the bus is at desired speed, the acceleration will effectively be zero, the same as if it where not moving so this would not be an ideal sensor to use A GPS measuring speed in any direction…
  • shabaz
    shabaz over 10 years ago in reply to gadget.iom +1
    That's true, but (been a long time since I was on a bus!) there are the 'smash glass' hammers or override buttons with thin glass in front of them. Maybe that is not an option in some countries though…
  • Former Member
    Former Member over 10 years ago in reply to balearicdynamics +1
    Yes okay. so basically I have an: 1. Arduino UNO 2. 3 Axis Gyroscope+Accelerome ter Module for Arduino MPU 6050 3. I have not still buy thew electric lock but what do you think of this: http://www.ebay…
Parents
  • mcb1
    mcb1 over 10 years ago

    Good idea to use your efforts in science.

     

    An alternative is to have the door controlling the vehicle.

    If the door is not shut the vehicle cannot move ...

     

    You could use an external sensor to detect movement of the vehicle completely independant of any systems on the vehicle.

    GPS or a IR laser to the roadway would detect movement.

     

    Any system you design will need to include several methods for fitting to various type of vehicles.

    However the final application should be outside of the scope of the project, since it will need to be fitted by a qualified Automotive Engineer.

     

    Our buses all have door on the side and they tend to open sideways, which minimises this tragedy.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 10 years ago

    Good idea to use your efforts in science.

     

    An alternative is to have the door controlling the vehicle.

    If the door is not shut the vehicle cannot move ...

     

    You could use an external sensor to detect movement of the vehicle completely independant of any systems on the vehicle.

    GPS or a IR laser to the roadway would detect movement.

     

    Any system you design will need to include several methods for fitting to various type of vehicles.

    However the final application should be outside of the scope of the project, since it will need to be fitted by a qualified Automotive Engineer.

     

    Our buses all have door on the side and they tend to open sideways, which minimises this tragedy.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 10 years ago in reply to mcb1

    Hello

    I am really pleased for your advice.

     

    Unfortunately, the bus do not have CAN.

    But i really wanted to try it with the accelerometer.

    Then i will see it it works or not, and i can learn from that.

     

    Do you have an idea how the sketch will be?

    I can also include an override switch to the driver just in case. And i will use a relay to operate the electric lock.

    Regards