Arduino Forum Data String Problem
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
  • Replies 5 replies
  • Subscribers 391 subscribers
  • Views 422 views
  • Users 0 members are here
Related

Data String Problem

aureta
aureta over 10 years ago

Hi, I am working with an Arduino sensor that gives out a series of three strings data that I want to visualize in the serial monitor. The problem I have is that as first printout at the SM the system returns a number (44 actually) that has nothing to do with the sensor readouts but is messes up the serial communication with another app I am writing in Python. How can I prevent that number 44 for being returned/printed, either from the Arduino or Python side ?. Thanks, Alejandro.

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago in reply to aureta +1
    Are you missing some of your setup code?
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    please post your sketch and we can better advise you

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • aureta
    aureta over 10 years ago in reply to Robert Peter Oakes

    Here it goes, thanks

     

     

     

    #include <Wire.h>

    #include "Adafruit_TCS34725.h"

    Adafruit_TCS34725 tcs = Adafruit_TCS34725(TCS34725_INTEGRATIONTIME_101MS, TCS34725_GAIN_4X);

    const int activationPin=13;

    const int sensorLEDpin= 3;

    const int lightpin=11;

     

    void setup(void) {

          pinMode(activationPin, OUTPUT);

          pinMode(sensorLEDpin, OUTPUT);

          pinMode(lightpin, OUTPUT);

          Serial.begin(9600);

     

    void loop(void)

    {

        digitalWrite(activationPin, HIGH);

        analogWrite(sensorLEDpin, 1);

        analogWrite(lightpin, 15);

        uint16_t r, g, b, c, colorTemp, lux; 

        tcs.getRawData(&r, &g, &b, &c);

        Serial.print(r,DEC); Serial.print(","); Serial.print(g,DEC); Serial.print(","); Serial.print(b,DEC);

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago in reply to aureta

    Are you missing some of your setup code?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to aureta

    So from reading Adafruit library examples

     

    your missing this

    if (tcs.begin()) {
       Serial.println("Found sensor");
      } else {
       Serial.println("No TCS34725 found ... check your connections");
       while (1);

      }

    in the setup

     

    have you tried the Adafruit samples provided with the library and do they work ok

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • aureta
    aureta over 10 years ago in reply to Robert Peter Oakes

    hi, thank you, finally I got it working, the issue was at the sensor library.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • aureta
    aureta over 10 years ago in reply to Robert Peter Oakes

    hi, thank you, finally I got it working, the issue was at the sensor library.