Arduino Forum Ultrasonic Receiver Circuit
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
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 402 subscribers
  • Views 1157 views
  • Users 0 members are here
  • components
  • circuit
  • receiver
  • ultrasonic
Related

Ultrasonic Receiver Circuit

Former Member
Former Member over 10 years ago

I wish to build the Arduino ultrasonic receiver circuit in the attached photo.  The circuit is in the book Arduino Circuits & Projects Guide (http://www.amazon.com/gp/product/1907920250?psc=1&redirect=true&ref_=oh_aui_detailpage_o01_s03).  The author recommend your site to purchase the components for the circuit (the author dose not provide a list of components).  I do not recognize items 1 & 2 in the circuit nor can I associate them with the schematic. 

 

Please tell me items 1 & 2 are in the circuit. 

 

Thank you,

 

David Sanford

 

 

image

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    Item 1 is an inductor and there are none in the schematic so it may have simply been sitting on the bread board but not wired up to anything (Probably used while experementing other things)

     

    item 2 is probably the 6n8 Capacitor based on its connection to the transducer on the bread board and the fact the other end of the ransducer seems to be grounded

     

    all of the components are available from the Newark / Farnell web site to purchase

     

    you do realize this is only a reciever, it will will require an ultrasonic transmitter to complete a usable toy / project unless your trying to pick up on stray or other ultrasonic signals in the vacinity

     

    hope this helps

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Robert Peter Oakes

    Thanks!   I'm building an IR/ultrasonic beacon system and the ultrasonic transmitter and receiver must function independently. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to Robert Peter Oakes

    Thanks!   I'm building an IR/ultrasonic beacon system and the ultrasonic transmitter and receiver must function independently.