Arduino Forum RTC combined with servo device
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
  • State Not Answered
  • Replies 8 replies
  • Subscribers 392 subscribers
  • Views 2229 views
  • Users 0 members are here
  • Design
Related

RTC combined with servo device

Former Member
Former Member over 10 years ago

Hello,

I have a project and part of it involve an RTC clock and a servo. see attachment below.

I already built the circuit but I am completely lost with the sketch.

The objective of the project is :

After every 3 hours the servo automatically rotate 60 degrees.

Hope you could help me in the sketch.

Thanks in advance!

 

image

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    Can you show us what you have so far Have your already tried getting the servo to work using the standard servo library, same question for the RTC What is the model of the servo, I would normally recommend…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Former Member +1
    You can make it change at what ever interval you like and as far as you like within its limits just write the program based on what info I provided and then share your results, and we can help further…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    So first things first (btw, you don't say what to do if and when the servo reaches 180deg or 360, do you stop, reset to zero, something else ?

     

    Ignore the RTC initially and simply setup an LONG variable to hold the current system time (mills() )

    every 60 seconds (60,000 mills) move the servo

     

    #define interval 60000

    #define changeAngle 60

    #define maxAngle 180

    #define minAngle 0

     

    long mytimer = 0;

    int myAngle = 0;

     

    setup()

    {

    ...

    mytimer = mills();

    }

    loop()

    {

    ...

    if (mills() - myvariable > interval)

         {

         myAngle += changeAngle

         if (myAngle >= maxAngle)  myAngle = minAngle; // protect servo and sanity image

         myservo.write(myAngle);

         mytimer = mills();                // setup timer for next loop

         }

    // now do other stuff

    }

     

    This is not tested , I simply put it from head to page as I thought of it so you may need to do some work on it but it shows you the basics of how to get what you want, now its up to you

    once you have this running, it will be a simple matter of changing the mills() to use the RTC and changing the values of the interval

     

    ... in setup and loop simply is where your other code may go, it is of course not valid in the real code

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Robert Peter Oakes

    in fact yes, since a servo can rotate only 180 degrees after 180 degress i wanted it to return to zero.


    ok yes so do you think every 1 minutes it can change 60 degrees?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to Former Member

    You can make it change at what ever interval you like and as far as you like within its limits

     

    just write the program based on what info I provided and then share your results, and we can help further

     

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to Former Member

    You can make it change at what ever interval you like and as far as you like within its limits

     

    just write the program based on what info I provided and then share your results, and we can help further

     

    Peter