I have a OLED LCD screen, I got in a lucky bag thingy at Maplins (for you Americans, its our local electronics shop). I have found a data sheet but not found it much use, on the unit there is a Few codes and numbers.
On the front there is the screen, then below a little bit of paper with the code " OS096016PP0MB2B10 " then below that there are two other codes " H3610 " and " 50824 ", also engraved on the back very faintly is has another code " D 8 1 8 B U 2 - 0 1 ".
Then below it there is the little ribbon cable.
If it helps it is a very small screen and I hope to use it in a project.
Any help (if any) is appreciated.