Arduino Forum Arduino Serial Port Problem
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
  • State Not Answered
  • Replies 15 replies
  • Subscribers 395 subscribers
  • Views 2257 views
  • Users 0 members are here
Related

Arduino Serial Port Problem

Former Member
Former Member over 10 years ago

Hello,

  I have a problem that is preventing me from using my arduino. The serial port only gives me four options ,( /dev/tty.Bluetooth-PDA-Sync , /dev/cu.Bluetooth-PDA-Sync , /dev/tty.Bluetooth-Modem ,and /dev/cu.Bluetooth-Modem )none of them of work.Before this happened,I downloaded the library from "Make an Arduino Controlled Robot" and ever since I have had my serial port problem.Does anyone know how to fix this or know anything else that might have caused it.

                       Please write back soon,

                                         LG

  • Sign in to reply
  • Cancel

Top Replies

  • bobalexander
    bobalexander over 10 years ago in reply to Former Member +2
    You should see: /dev/tty.usbmodem621 or /dev/tty.usbserial-A02f8e It most likely will not say anything about Arduino... Are you going through a USB hub or directly in? Do you have anything connected to…
  • screamingtiger
    screamingtiger over 10 years ago +1
    What OS are you using? Linux? ALso what is giving you those options, the arduino IDE?
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to Former Member +1
    Hi Lucas, As I was supposing with the Arduino UNO no drivers are needed, accordingly with the UNO installation notes on Max. Please take a look to this link https://www.arduino.cc/en/Guide/MacOSX and double…
Parents
  • Former Member
    0 Former Member over 10 years ago

    Sorry I have not responded sooner. I tried what you recomended but it sadly didn't work.

                             -Lucas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to Former Member

    Lucas,

     

    I had a problem very similar on an Arduino compatible (built by me) and I have discovered some things.

     

    Yosemite 10.9 (and OS X 10.10 and newer) requires a signed USB driver kext (kernel extension). You can find one on the FTDI web site here:

    http://www.ftdichip.com/Drivers/VCP.htm

    Use version 2.3 for 64-bit OS X 10.9 or later. Install and reboot. Plug in your Arduino, and the Terminal command:

    /usr/sbin/kextstat | grep FTDI

    This will tell you if the FTDI VCP driver actually loaded. Also a /dev/tty.usbserial-xxxxxxxx entry should appear in your /dev directory.

    If not,the Mac USB port isn't talking to your Arduino. So it's no use trying the Arduino IDE application.

    Let me know if this workaround will work.

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to balearicdynamics

    Yosemite 10.9 (and OS X 10.10 and newer) requires a signed USB driver

    There was a similar problem with windows 8.1

     

    The solution was to choose a Comm Port and then point to the Arduino driver.

    This was much easier than ignoring unsigned drivers, etc.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to mcb1

    I have not yet had the luck to paly with windows 8, but Mac has a linux oriented approach while Windows 8 I think it is different.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to mcb1

    I have not yet had the luck to paly with windows 8, but Mac has a linux oriented approach while Windows 8 I think it is different.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 10 years ago in reply to balearicdynamics

    not yet had the luck to play with windows 8

    That's not exactly how I would phrase it ....

     

    I can live with Windows 7 for quite some time.

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to mcb1

    I see. It was ironic image