Arduino Forum Arduino Serial Port Problem
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
  • State Not Answered
  • Replies 15 replies
  • Subscribers 395 subscribers
  • Views 2257 views
  • Users 0 members are here
Related

Arduino Serial Port Problem

Former Member
Former Member over 10 years ago

Hello,

  I have a problem that is preventing me from using my arduino. The serial port only gives me four options ,( /dev/tty.Bluetooth-PDA-Sync , /dev/cu.Bluetooth-PDA-Sync , /dev/tty.Bluetooth-Modem ,and /dev/cu.Bluetooth-Modem )none of them of work.Before this happened,I downloaded the library from "Make an Arduino Controlled Robot" and ever since I have had my serial port problem.Does anyone know how to fix this or know anything else that might have caused it.

                       Please write back soon,

                                         LG

  • Sign in to reply
  • Cancel

Top Replies

  • bobalexander
    bobalexander over 10 years ago in reply to Former Member +2
    You should see: /dev/tty.usbmodem621 or /dev/tty.usbserial-A02f8e It most likely will not say anything about Arduino... Are you going through a USB hub or directly in? Do you have anything connected to…
  • screamingtiger
    screamingtiger over 10 years ago +1
    What OS are you using? Linux? ALso what is giving you those options, the arduino IDE?
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to Former Member +1
    Hi Lucas, As I was supposing with the Arduino UNO no drivers are needed, accordingly with the UNO installation notes on Max. Please take a look to this link https://www.arduino.cc/en/Guide/MacOSX and double…
Parents
  • screamingtiger
    0 screamingtiger over 10 years ago

    What OS are you using?  Linux?  ALso what is giving you those options, the arduino IDE?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to screamingtiger

    First of all thank you for responding to my question.I am using Mac 10.6.8. and and the Arduino IDE gave me these options.

                                            -Lucas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to screamingtiger

    First of all thank you for responding to my question.I am using Mac 10.6.8. and and the Arduino IDE gave me these options.

                                            -Lucas