Arduino Forum Two Tone Sequential Page Decoding
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 392 subscribers
  • Views 678 views
  • Users 0 members are here
  • tonedecoder
  • arduino
Related

Two Tone Sequential Page Decoding

bryaneades@yahoo.com
bryaneades@yahoo.com over 10 years ago

I'm researching the LM567 tone decoder circuit and find that I will need four circuits for a project. I'm wondering if an Arduino would better suit my needs.

 

I have an Arduino hooked to a decoding circuit now that works in this way:

 

Three frequency pairs are used to initiate three different functions. Frequency A is active for .5 seconds then frequency B for 2 seconds in secession. The decoder has an output that goes low for .5 seconds. This activates a function on an arduino via an input pin. Frequency A and frequency C initiates a different function. Frequency A and frequency D initiate a third function.

 

Can Arduino be used to decode these frequencies and then run the corresponding function. My project could be reduced to just a single Arduino Uno.

 

I've seen some examples on the internet using circuitry that could be on a shield protoboard to convert the sine wave to a square wave. Then the Arduino counts the pulses, but that programming is way over my head. 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    Cool

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    Cool