Arduino Forum Hands-on learning(Help a newbie)
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
  • State Suggested Answer
  • Replies 16 replies
  • Answers 2 answers
  • Subscribers 392 subscribers
  • Views 942 views
  • Users 0 members are here
  • android
  • help
  • arduino
  • newbie
Related

Hands-on learning(Help a newbie)

Former Member
Former Member over 10 years ago

     As mentioned, I'm completely a newbie to this field except for maybe blinking LEDs and stuff. This project I wish to do is not a school assignment. It is just a learning project I wish to do. I have        an idea in mind and would like your help to know whether it is feasible and if yes, how do i go about it.

 

     Project Aim: To create a system that turns off current to your mobile battery(Android {android.os.BatteryManager} ) if it reads a certain battery level. Any variations of this would be fine too. Like start charging if battery level < 20%.

 

    Any help would be much appreciated.Links to resources.Direct help pertaining to project as in components required, prerequisite knowledge required, expected challenges. Anything basically.

 

      I'm new to this community as well. Hope to make some friends along the way. Thank you.
                                                                                                                                                        --Hasmit.
  • Sign in to reply
  • Cancel
Parents
  • m.ratcliffe
    0 m.ratcliffe over 10 years ago

    Most smart phones already stop charging when full, turning the mains off will offer very little savings [maybe even less than the extra power consumption of the arduino watcher] and you will probably be playing with mains electricity. If it is a cool first learning project you want to work on I would advice something a bit more fun and low voltage that also lets you mess around with the code to see changes. For example something with feedback loops that you can change the control strategy and see the real world effect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to m.ratcliffe

    Agree, besides, if the battery was disconnected by an external circuit, then the mobile phone battery would be undergoing unnecessary charge/discharge cycles which is pretty bad especially for mobile phones with a non-removable battery (yuk).

    Instead, better to leave the technicalities to the on-board power management circuit which is designed to switch off and prevent battery over-charge and it continues to use USB connected power when the battery has charged, to run the phone.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to shabaz


    Thank you Shabaz for the suggestion.

    Could you please take time out to suggest alternative projects that I may be able to implement such that they also have a real world purpose?

                                                                                                        Thank you in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to shabaz


    Thank you Shabaz for the suggestion.

    Could you please take time out to suggest alternative projects that I may be able to implement such that they also have a real world purpose?

                                                                                                        Thank you in advance.