Arduino Forum Hands-on learning(Help a newbie)
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
  • State Suggested Answer
  • Replies 16 replies
  • Answers 2 answers
  • Subscribers 392 subscribers
  • Views 942 views
  • Users 0 members are here
  • android
  • help
  • arduino
  • newbie
Related

Hands-on learning(Help a newbie)

Former Member
Former Member over 10 years ago

     As mentioned, I'm completely a newbie to this field except for maybe blinking LEDs and stuff. This project I wish to do is not a school assignment. It is just a learning project I wish to do. I have        an idea in mind and would like your help to know whether it is feasible and if yes, how do i go about it.

 

     Project Aim: To create a system that turns off current to your mobile battery(Android {android.os.BatteryManager} ) if it reads a certain battery level. Any variations of this would be fine too. Like start charging if battery level < 20%.

 

    Any help would be much appreciated.Links to resources.Direct help pertaining to project as in components required, prerequisite knowledge required, expected challenges. Anything basically.

 

      I'm new to this community as well. Hope to make some friends along the way. Thank you.
                                                                                                                                                        --Hasmit.
  • Sign in to reply
  • Cancel
Parents
  • m.ratcliffe
    0 m.ratcliffe over 10 years ago

    Most smart phones already stop charging when full, turning the mains off will offer very little savings [maybe even less than the extra power consumption of the arduino watcher] and you will probably be playing with mains electricity. If it is a cool first learning project you want to work on I would advice something a bit more fun and low voltage that also lets you mess around with the code to see changes. For example something with feedback loops that you can change the control strategy and see the real world effect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to m.ratcliffe

      Thank you for the reply Michael. Yes, I am aware that almost all modern day Li-ion batteries possess an internal mechanism to achieve what i want to do. However I thought it would be fun to implement it. Nonetheless, Would you be kind enough to suggest something fun but with a learning curve to it? Preferably something to do with Android/Smartphones in general since I could not find a lot of projects that have already been done on the same.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to m.ratcliffe

      Thank you for the reply Michael. Yes, I am aware that almost all modern day Li-ion batteries possess an internal mechanism to achieve what i want to do. However I thought it would be fun to implement it. Nonetheless, Would you be kind enough to suggest something fun but with a learning curve to it? Preferably something to do with Android/Smartphones in general since I could not find a lot of projects that have already been done on the same.