Arduino
  • Products
  • More
Arduino
Arduino Forum RTC DS1307 not working with Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 417 subscribers
  • Views 3400 views
  • Users 0 members are here
Related

RTC DS1307 not working with Arduino

e14 Contributor
e14 Contributor over 11 years ago

I am currently trying to interface an RTC with arduino. For this purpose,I am using Tiny RTC module DS1307 purchased from Ebay

My connections are as follows-

Vcc-Vcc

GND-GND

SCL-A5

SDA-A4

 

 

I have downloaded the RTC library from adafruit website and am trying the example code.

 

 

#include <Wire.h>

#include "RTClib.h"

RTC_DS1307 RTC;

 

 

void setup () {

    Serial.begin(9600);

    Wire.begin();

    RTC.begin();

  if (! RTC.isrunning()) {

    Serial.println("RTC is NOT running!");

    // following line sets the RTC to the date & time this sketch was compiled

    RTC.adjust(DateTime(__DATE__, __TIME__));

  }

}

void loop () {

    DateTime now = RTC.now();

    Serial.print(now.year(), DEC);

    Serial.print('/');

    Serial.print(now.month(), DEC);

    Serial.print('/');

    Serial.print(now.day(), DEC);

    Serial.print(' ');

    Serial.print(now.hour(), DEC);

    Serial.print(':');

    Serial.print(now.minute(), DEC);

    Serial.print(':');

    Serial.print(now.second(), DEC);

    Serial.println();

    delay(1000);

}

 

Below is the Screenshot of the output I am getting using Serial monitor. I want to ask why does the output(date and time) come correct for the first time and after that becomes incorrect? I am really confused.

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    Second issue is the way your setting and getting the compile time, if you use the Adafruit library (Not sure if they wrote it but who cares right now)  https://github.com/adafruit/RTClib and look at the softrtc example, it works correctly

     

    here is a clip of it

     

    void setup () {
        Serial.begin(57600);
        // following line sets the RTC to the date & time this sketch was compiled
        rtc.begin(DateTime(F(__DATE__), F(__TIME__)));
        // This line sets the RTC with an explicit date & time, for example to set
        // January 21, 2014 at 3am you would call:
        // rtc.adjust(DateTime(2014, 1, 21, 3, 0, 0));
    }

     

    so between switching the A4 and A5, and changing the code, it should now work

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jsw247
    0 jsw247 over 6 years ago in reply to Robert Peter Oakes

    I know this is an old thread , but I have a fix for this , there is nothing wrong with the code .

    the board has a incorrectly designed connection between RTC chip and backup battery , the fix is remove R4 R6 and D1 , Short R6 connections out , this should give you full battery voltage of 3.2 volts on the RTC chip PIn 3 .Whoever designed this put a 510k resistor in series between the battery and RTC chip , with a diode feeding from 5v .This goes against the manufacturers recommended circuit diagram

     

     

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jsw247
    0 jsw247 over 6 years ago in reply to Robert Peter Oakes

    I know this is an old thread , but I have a fix for this , there is nothing wrong with the code .

    the board has a incorrectly designed connection between RTC chip and backup battery , the fix is remove R4 R6 and D1 , Short R6 connections out , this should give you full battery voltage of 3.2 volts on the RTC chip PIn 3 .Whoever designed this put a 510k resistor in series between the battery and RTC chip , with a diode feeding from 5v .This goes against the manufacturers recommended circuit diagram