Arduino Forum Using the Garmin 16x HVS GPS with Arduino
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
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 402 subscribers
  • Views 563 views
  • Users 0 members are here
Related

Using the Garmin 16x HVS GPS with Arduino

maquinna
maquinna over 10 years ago

I want to use a Garmin 16x HVS gps receiver with  a Leonardo Arduino board. Basically I would solder a db9 connector to the serial comport input and output. I want to control the output from the gps receiver. I want  to compare the most recent gps string with the one before and if the position has not change by 50 feet(programmeable 0 to 100 feet) the gps string would not be sent through the output  serial port. How would I code this?

  • Sign in to reply
  • Cancel
Parents
  • screamingtiger
    0 screamingtiger over 10 years ago

    So I assume you know how to hook it up to the GPS.

    Please see TinyGPS++ for Arduino.

     

    https://github.com/mikalhart/TinyGPSPlus/releases/tag/v0.94b

     

    Inside you will find examples on how to read from the serial, using such things as Serial.begin(9600) or the baud rate you want to use.

     

    The NMEA sentences are parsed for you, and it gives you coordinates and other information. You can check a flag when each time the coordinates are updated.  There is a function called "DistanceBetween" that takes two set of coordinates and computes the distance between them using an arclength method, which they refer to as the "Great Circle Problem".

     

    There are also a set of NMEA commands you can send that GPS.  Please see http://www.gpsinformation.org/dale/nmea.htm for more information.  The hard part will just be determining what baud rate it defaults to.

     

    Go have a look and come back if you want more examples.  If you like my answer, please mark it helpful and/or correct.

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • maquinna
    0 maquinna over 10 years ago in reply to screamingtiger

    Thank you. You have been very helpful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • maquinna
    0 maquinna over 10 years ago in reply to screamingtiger

    Thank you. You have been very helpful.