Arduino Forum hello
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
  • State Not Answered
  • Replies 16 replies
  • Subscribers 392 subscribers
  • Views 1061 views
  • Users 0 members are here
Related

hello

Former Member
Former Member over 10 years ago

image

Dear Sir;

I hope this email find you well. I have question about the needed parts for practicing PWM on motor operate on 5-18 voltage. I have arduino and Motor control shield for arduino. Is these two parts enough or I need other parts.

best greetings

Sazan

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 10 years ago in reply to Jan Cumps +1
    really thank you very much
Parents
  • Jan Cumps
    0 Jan Cumps over 10 years ago

    Sazan, the only additional thing you need is a power supply - and a motor. You'll have to provide the 5-18 volts to the controller board from separate power.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Jan Cumps

    thank you for answer

    the motor I have has the attached datasheet. Is it good to use it with ardunio? or I have to change it .

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to Jan Cumps

    thank you for answer

    the motor I have has the attached datasheet. Is it good to use it with ardunio? or I have to change it .

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to Former Member

    You can use that motor. As power supply, you need something that can deliver 18 V and 55 mA dc - I'd go for 100 mA

     

    EDIT: (I saw that this is NO LOAD current)

    You didn't show the current vs voltage graph of your motor (it should be the graph just below the piece of the pdf you uploaded - other motors in that series go up to 1.5A).

     

     

     

    It will work on lower voltages, but you won't be able to use the motor at full force then.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to Jan Cumps

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Jan Cumps

    thank you.

    really I want to change the input voltage and read the output voltage. I want to convert the rpm speed to voltage. could you please instruct me in  steps how to connect the motor and read its input voltage and output voltage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Former Member

    in your opinion. what should I do. Really I need help lam lost

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to Former Member

    From the photo of your motor shield, it seems that you have the Adafruit Motor/Stepper/Servo Shield for Arduino kit - v1.2 - or a clone.

     

    https://www.adafruit.com/products/81

     

    They have a tutorial: https://learn.adafruit.com/adafruit-motor-shield

     

    Follow the steps on the left side of that page. Start from the begin. Once you reach the 'Use It' section, follow the library install, Power Usage and Using DC motors parts of the tutorial.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Jan Cumps

    really thank you very muchimageimageimageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Former Member

    ok so the motor will not work at full power. I will connect the motor to signal generator. The motor will rotate, the ardunio connected to the computer power only. By using photo sensor I can find the rpm (speed).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Jan Cumps

    ok so the motor will not work at full power. I will connect the motor to signal generator. The motor will rotate, the ardunio connected to the computer power only. By using photo sensor I can find the rpm (speed).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Jan Cumps

    but still I did not find a way how to read the signal generator input voltage to dc motor by ardunio , Is the any way to prevent ardunio damage.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to Former Member

    sazan , you should not have to use a signal generator. The Arduino and Motor shield will generate the signal for the motor.

     

    Can you make and upload a drawing of how you are going to connect the motor to the shield, and how you are going to connect your external power supply to the shield?

    My advise is to really follow the adafruit guide step by step, without skipping a single point.

    It contains everything: electrical connections, library install, sketch to test the motor.

     

    Try to finish the tutorial and don't give up until you have it working. Your motor should run forwards for a second, run backwards one second, and stop for one second.

    When you are at that point, you can think about next steps.