Arduino Forum Using OpenCV
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
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 402 subscribers
  • Views 910 views
  • Users 0 members are here
  • opencv
  • arduino
  • software
Related

Using OpenCV

timswift
timswift over 10 years ago

Hi

 

I have ben wanting to try object tracking with a Arduino and openCV for some time now but I can not get openCV to open.

Do I need more software to run it?

 

 

thanks

 

tim

  • Sign in to reply
  • Cancel
Parents
  • cstanton
    0 cstanton over 10 years ago

    OpenCV requires a computer with an operating system to run, typically.

     

    It compiles from C++ and/or Python.

     

    So its typical to use a RaspberryPi, for example, to handle OpenCV processing and then get the Arduino to do whatever you want in communication from the Pi.

     

    You could port the code over to implement it in hardware or bare metal, but that's going to take a lot of work and you're probably making life difficult for yourself, not only with trying to find the suitable hardware to do it but also converting the software.

     

    You can read more about OpenCV here: OpenCV | OpenCV .

     

    It may be a good idea to flip your request on its head:

    What are you trying to achieve?

    What do you want to do with OpenCV?

    What hardware do you hope to use?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • timswift
    0 timswift over 10 years ago in reply to cstanton

    I wanted to run it on my PC and then interface it with a Arduino two servos and a USB camera to track objects.

     

    Would Visual Studio Express work as a compiler?

    tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • timswift
    0 timswift over 10 years ago in reply to cstanton

    I wanted to run it on my PC and then interface it with a Arduino two servos and a USB camera to track objects.

     

    Would Visual Studio Express work as a compiler?

    tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • cstanton
    0 cstanton over 10 years ago in reply to timswift

    For compiling code for your Arduino, no, it lacks avr-gcc by default which is the C compiler for the typical Arduino microprocessor.

     

    Unless you use something like http://playground.arduino.cc/Code/VisualMicro Visual Micro which is a plugin that adds/uses the compiler.

     

    As for OpenCV, you can compile it using VisualStudio: http://docs.opencv.org/doc/tutorials/introduction/windows_install/windows_install.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer