Arduino Forum Need 10 minutes from an Arduino Expert
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
  • State Verified Answer
  • Replies 34 replies
  • Subscribers 394 subscribers
  • Views 2252 views
  • Users 0 members are here
  • arduino
Related

Need 10 minutes from an Arduino Expert

gub11
gub11 over 10 years ago

Having some noob trouble with a sketch, and an arduino uno, i'm sure anybody with more knowledge than me could help.

add me on skype, gabe.spound2

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to gub11 +2
    The people trying to help here are all over the world.. literally so many different time zones, we get to respond when we have a moment from our busy lives and as a principal we dont skype etc, this would…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    Can you please simply post your issue here with sketch, diagrams and description of the problem then many folks will be able to help and then the answer will also help many
  • mcb1
    mcb1 over 10 years ago in reply to gub11 +1
    gub11 Okay so you've included the code for the LED. What about including what you did for the relay. Note to include code paste the code, then select it. Click on the >> and then select Syntax highlighting…
Parents
  • gub11
    0 gub11 over 10 years ago

    can somebody just skype with me for five minutes, im sure its a simple issue, i just don't know much

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to gub11

    The people trying to help here are all over the world.. literally so many different time zones, we get to respond when we have a moment from our busy lives and as a principal we dont skype etc, this would lead us to not getting other things done, if you, then the next etc. and it would never be just 5mins, we have way too much experiance with these things to assume only 5mins would be enough

     

    + as already stated, this is a community and we help the community and expect the responses to be shared with the community. putting things here helps people see a history of the issue, how it was resolved etc. + by getting you to walk through it, you will also learn much more.

     

    I am sorry if we seem to be a pain by making you do it this way but the other 200,000+++ folks are quite happy to conform, please understand, nothing personal, just the right way to move forward

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gub11
    0 gub11 over 10 years ago in reply to Robert Peter Oakes

    Robert Peter Oakesmcb1balearicdynamics

     

    Sorry for the misuse of the forum, i was being lazy and i apologize.

    I have attatched a schematic i made in fritzing(it's my first one so it might be a little messy, but its legible.  And i have linked a video of the issue.

    the relay turns the led on and off, instead of one clap for off, and another for on, the code im using is also in an above post.  I am really at a loss for what the issue is because if i cut out the relay, and just wire pin 2 to the positive connection of the led, it works just fine, on with a clap, off with another, but when its hooked up to the relay, it just goes on and off with one clap.

    https://youtu.be/KMs2VD4fwFA

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gub11
    0 gub11 over 10 years ago in reply to gub11

    *Bump* this is also open to anybody else who wasn't mentioned above, i really need help with this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gub11
    0 gub11 over 10 years ago in reply to gub11

    *Bump* this is also open to anybody else who wasn't mentioned above, i really need help with this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to gub11

    Hi Gabriel,

     

    I subscribe the hypothesysof jw0752 But let me know a couple of details:

     

    1. Are you powering the relay with 3.3 V or 5V from Arduino ?
    2. Check the relay data sheet what is the drawing power
    3. Are you using the relay also to power the led when it switches?

     

    If 3. is true, I suggest that as should be done in the normal use, the Relay is just to use a low power (Arduino 5V) to switch the coil then the other side will use an external power to manage the device. If you leave the circuit as-it it is also possible it works with a LED but it is formerly wrong as the Relay is not used to power anything else (e.g. a motor or a more power device, like a 12V fan).

     

    Take a look to the following schematics. This is the correct use of the Relay (it is a 5V powered relay so it will work fine with the Arduino power out) and is used to switch an external power supply. The relay area is highlighted in the red rectangle.

     

    Enrico

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gub11
    0 gub11 over 10 years ago in reply to balearicdynamics

    1, 5v

    2, idk what that means

    3, i think im using the relay to power the led, im still not 100% how relays work, but when the switch is connected in the relay, power goes through it to the led