Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Using multiple MFRC522 RFID readers on one Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 3 answers
  • Subscribers 419 subscribers
  • Views 30517 views
  • Users 0 members are here
  • mfrc522
  • rfid
Related

Using multiple MFRC522 RFID readers on one Arduino

e14 Contributor
e14 Contributor over 11 years ago

I'm still pretty new to this, but I'm trying to connect up to 12 MFRC522 RFID readers to my arduino uno. They're the cheap under $5 ones from ebay. I can get one to work using the miguelbalboa/rfid library but I can't seem to get a second one working. I've attached the code I'm trying to use. Both readers are sharing the same MOSI, MISO, and SCK pins. The library I'm trying to use is found at https://github.com/miguelbalboa/rfid

 

MOSI pin 11

MISO pin12

SCK  pin 13

 

#include <SPI.h>

#include <MFRC522.h>

 

#define RST_PIN 7 //

#define RST_PIN2  8    // Configurable, see typical pin layout above

#define SS_PIN 9 //

#define SS_PIN2   10    // Configurable, see typical pin layout above

 

MFRC522 mfrc522(SS_PIN, RST_PIN); // Create MFRC522 instance

MFRC522 mfrc522_2(SS_PIN2, RST_PIN2);   // Create MFRC522 instance.

 

 

void setup() {

Serial.begin(9600); // Initialize serial communications with the PC

while (!Serial); // Do nothing if no serial port is opened (added for Arduinos based on ATMEGA32U4)

SPI.begin(); // Init SPI bus

mfrc522.PCD_Init(); // Init MFRC522

mfrc522_2.PCD_Init(); // Init MFRC522

ShowReaderDetails(); // Show details of PCD - MFRC522 Card Reader details

Serial.println(F("Scan PICC to see UID, type, and data blocks..."));

}

 

void loop() {

// Look for new cards

if ( ! mfrc522.PICC_IsNewCardPresent()) {

return;

}

 

// Select one of the cards

if ( ! mfrc522.PICC_ReadCardSerial()) {

return;

}

 

 

// Dump debug info about the card; PICC_HaltA() is automatically called

mfrc522.PICC_DumpToSerial(&(mfrc522.uid));

 

  delay(1000);

 

  // Look for new cards

  if ( ! mfrc522_2.PICC_IsNewCardPresent()) {

    return;

  }

 

  // Select one of the cards

  if ( ! mfrc522_2.PICC_ReadCardSerial()) {

    return;

  }

 

  // Dump debug info about the card; PICC_HaltA() is automatically called

  mfrc522_2.PICC_DumpToSerial(&(mfrc522.uid));

}

 

void ShowReaderDetails() {

// Get the MFRC522 software version

byte v = mfrc522.PCD_ReadRegister(mfrc522.VersionReg);

Serial.print(F("MFRC522 Software Version: 0x"));

Serial.print(v, HEX);

if (v == 0x91)

Serial.print(F(" = v1.0"));

else if (v == 0x92)

Serial.print(F(" = v2.0"));

else

Serial.print(F(" (unknown)"));

Serial.println("");

// When 0x00 or 0xFF is returned, communication probably failed

if ((v == 0x00) || (v == 0xFF)) {

Serial.println(F("WARNING: Communication failure, is the MFRC522 properly connected?"));

}

byte w = mfrc522_2.PCD_ReadRegister(mfrc522_2.VersionReg);

Serial.print(F("MFRC522_2 Software Version: 0x"));

Serial.print(w, HEX);

if (w == 0x91)

    Serial.print(F(" = v1.0"));

else if (w == 0x92)

    Serial.print(F(" = v2.0"));

else

    Serial.print(F(" (unknown)"));

Serial.println("");

// When 0x00 or 0xFF is returned, communication probably failed

if ((w == 0x00) || (v == 0xFF)) {

   Serial.println(F("WARNING: Communication failure, is the MFRC522 properly connected?"));

  }

}

 

I'm not opposed to using more than one arduino, because I'm going to have it feed information to a raspberry pi. I would prefer to use as few as possible.

 

Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • butcher97
    butcher97 over 6 years ago +3 suggested
    I know this is very late, but i am hoping this will help someone at a later date. The issue with these MFRC522 boards is that they are not very well designed to work with other boards on the same SPI bus…
  • tpra
    tpra over 5 years ago in reply to butcher97 +2
    I registered just to say thank you. Many, many thanks for this one.
  • beacon_dave
    beacon_dave over 10 years ago in reply to jeroenb42 +1 suggested
    Have you checked that only one SPI slave select line is active at any one time ?
Parents
  • Abhignan_Rakshith_Main
    0 Abhignan_Rakshith_Main over 4 years ago

    This is the updated Arduino code for 2 RFID'S !

    #include <SPI.h>

    #include <MFRC522.h>

    #define RST_PIN 9

    #define RST_PIN2 3 // Configurable, see typical pin layout above

    #define SS_PIN 10

    #define SS_PIN2 8 // Configurable, see typical pin layout above

    MFRC522 mfrc522(SS_PIN, RST_PIN); // Create MFRC522 instance

    MFRC522 mfrc522_2(SS_PIN2, RST_PIN2); // Create MFRC522 instance.


    void ShowReaderDetails();
    bool rfid1= LOW;
    bool rfid2 = HIGH;

    void setup() {

    Serial.begin(9600); // Initialize serial communications with the PC

    while (!Serial); // Do nothing if no serial port is opened (added for Arduinos based on ATMEGA32U4)

    SPI.begin(); // Init SPI bus

    mfrc522.PCD_Init(); // Init MFRC522

    mfrc522_2.PCD_Init(); // Init MFRC522

    ShowReaderDetails(mfrc522); // Show details of PCD - MFRC522 Card Reader details
    ShowReaderDetails(mfrc522_2); // Show details of PCD - MFRC522 Card Reader details
    Serial.println(F("Scan PICC to see UID, type, and data blocks..."));

    }

    void loop() {

    // Look for new cards

    if ( ! mfrc522.PICC_IsNewCardPresent() ) {

    rfid1=LOW;

    //return;

    }else
    {
    rfid1 =HIGH;
    }
    // Select one of the cards

    if ( ! mfrc522.PICC_ReadCardSerial() ) {

    rfid1 = LOW;
    // return;

    }else
    {
    rfid1 =HIGH;
    }


    // Dump debug info about the card; PICC_HaltA() is automatically called
    if(rfid1)
    {
    mfrc522.PICC_DumpToSerial(&(mfrc522.uid));
    rfid1 = LOW;
    }

    if ( ! mfrc522_2.PICC_IsNewCardPresent() ) {

    rfid2=LOW;

    //return;

    }else
    {
    rfid2 =HIGH;
    }
    // Select one of the cards

    if ( ! mfrc522_2.PICC_ReadCardSerial() ) {

    rfid2 = LOW;
    // return;

    }else
    {
    rfid2 =HIGH;
    }


    // Dump debug info about the card; PICC_HaltA() is automatically called
    if(rfid2)
    {
    mfrc522_2.PICC_DumpToSerial(&(mfrc522_2.uid));
    rfid2 = LOW;
    }
    }

    void ShowReaderDetails(MFRC522 rfid ) {

    // Get the MFRC522 software version

    byte v = rfid.PCD_ReadRegister(rfid.VersionReg);

    Serial.print(F("MFRC522 Software Version: 0x"));

    Serial.print(v, HEX);

    if (v == 0x91)

    Serial.print(F(" = v1.0"));

    else if (v == 0x92)

    Serial.print(F(" = v2.0"));

    else

    Serial.print(F(" (unknown)"));

    Serial.println("");

    // When 0x00 or 0xFF is returned, communication probably failed

    if ((v == 0x00) || (v == 0xFF)) {

    Serial.println(F("WARNING: Communication failure, is the MFRC522 properly connected?"));

    }

    byte w = rfid.PCD_ReadRegister(rfid.VersionReg);

    Serial.print(F("MFRC522_2 Software Version: 0x"));

    Serial.print(w, HEX);

    if (w == 0x91)

    Serial.print(F(" = v1.0"));

    else if (w == 0x92)

    Serial.print(F(" = v2.0"));

    else

    Serial.print(F(" (unknown)"));

    Serial.println("");

    // When 0x00 or 0xFF is returned, communication probably failed

    if ((w == 0x00) || (v == 0xFF)) {

    Serial.println(F("WARNING: Communication failure, is the MFRC522 properly connected?"));

    }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Abhignan_Rakshith_Main
    0 Abhignan_Rakshith_Main over 4 years ago

    This is the updated Arduino code for 2 RFID'S !

    #include <SPI.h>

    #include <MFRC522.h>

    #define RST_PIN 9

    #define RST_PIN2 3 // Configurable, see typical pin layout above

    #define SS_PIN 10

    #define SS_PIN2 8 // Configurable, see typical pin layout above

    MFRC522 mfrc522(SS_PIN, RST_PIN); // Create MFRC522 instance

    MFRC522 mfrc522_2(SS_PIN2, RST_PIN2); // Create MFRC522 instance.


    void ShowReaderDetails();
    bool rfid1= LOW;
    bool rfid2 = HIGH;

    void setup() {

    Serial.begin(9600); // Initialize serial communications with the PC

    while (!Serial); // Do nothing if no serial port is opened (added for Arduinos based on ATMEGA32U4)

    SPI.begin(); // Init SPI bus

    mfrc522.PCD_Init(); // Init MFRC522

    mfrc522_2.PCD_Init(); // Init MFRC522

    ShowReaderDetails(mfrc522); // Show details of PCD - MFRC522 Card Reader details
    ShowReaderDetails(mfrc522_2); // Show details of PCD - MFRC522 Card Reader details
    Serial.println(F("Scan PICC to see UID, type, and data blocks..."));

    }

    void loop() {

    // Look for new cards

    if ( ! mfrc522.PICC_IsNewCardPresent() ) {

    rfid1=LOW;

    //return;

    }else
    {
    rfid1 =HIGH;
    }
    // Select one of the cards

    if ( ! mfrc522.PICC_ReadCardSerial() ) {

    rfid1 = LOW;
    // return;

    }else
    {
    rfid1 =HIGH;
    }


    // Dump debug info about the card; PICC_HaltA() is automatically called
    if(rfid1)
    {
    mfrc522.PICC_DumpToSerial(&(mfrc522.uid));
    rfid1 = LOW;
    }

    if ( ! mfrc522_2.PICC_IsNewCardPresent() ) {

    rfid2=LOW;

    //return;

    }else
    {
    rfid2 =HIGH;
    }
    // Select one of the cards

    if ( ! mfrc522_2.PICC_ReadCardSerial() ) {

    rfid2 = LOW;
    // return;

    }else
    {
    rfid2 =HIGH;
    }


    // Dump debug info about the card; PICC_HaltA() is automatically called
    if(rfid2)
    {
    mfrc522_2.PICC_DumpToSerial(&(mfrc522_2.uid));
    rfid2 = LOW;
    }
    }

    void ShowReaderDetails(MFRC522 rfid ) {

    // Get the MFRC522 software version

    byte v = rfid.PCD_ReadRegister(rfid.VersionReg);

    Serial.print(F("MFRC522 Software Version: 0x"));

    Serial.print(v, HEX);

    if (v == 0x91)

    Serial.print(F(" = v1.0"));

    else if (v == 0x92)

    Serial.print(F(" = v2.0"));

    else

    Serial.print(F(" (unknown)"));

    Serial.println("");

    // When 0x00 or 0xFF is returned, communication probably failed

    if ((v == 0x00) || (v == 0xFF)) {

    Serial.println(F("WARNING: Communication failure, is the MFRC522 properly connected?"));

    }

    byte w = rfid.PCD_ReadRegister(rfid.VersionReg);

    Serial.print(F("MFRC522_2 Software Version: 0x"));

    Serial.print(w, HEX);

    if (w == 0x91)

    Serial.print(F(" = v1.0"));

    else if (w == 0x92)

    Serial.print(F(" = v2.0"));

    else

    Serial.print(F(" (unknown)"));

    Serial.println("");

    // When 0x00 or 0xFF is returned, communication probably failed

    if ((w == 0x00) || (v == 0xFF)) {

    Serial.println(F("WARNING: Communication failure, is the MFRC522 properly connected?"));

    }

    }