Arduino Forum Help with Home Automation
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
  • State Not Answered
  • Replies 18 replies
  • Subscribers 400 subscribers
  • Views 1208 views
  • Users 0 members are here
Related

Help with Home Automation

Former Member
Former Member over 10 years ago

Hello all,

 

I am a self taught coder and tech guy, Im looking to incorporate some home automation within my home. To start with I would like be able to control some LED strips from a internet portal just like this:

 

https://www.youtube.com/watch?v=n6u-H1sza-w

 

I really like this idea, however here are my issues

 

1 - I want a few of these around the living room and kitchen so having a pi per led will be expensive.

 

2 - I also want to be able to control the pre programmed set up's e.g. strobe, flash etc.

 

Here are my thoughts:

 

Arduino contected to the controller buttons that I will be using that sends a IR to the strip at close range (1 arduino per strip). All I need to know is what is the best way to control the ardunio over the internet. Im not worried that I will have to use 1 power socket per strip and unit.

 

Heres the other issue, I want to be able to build of this web portal and need it PHP so that the URL will not change when a button is clicked.

 

can anyone assist?

 

Regards - Aiden

 

UPDATE:

 

So I have the IR codes for the LED strips, This is what I need to do now,

 

Code them into the arduino with a LED emitter, test to make sure its working.

 

After that has been found to work, I then need to link a it to wifi for wireless access

 

Then I need to build a small control panel to control over the internet.

 

Thank,

Aiden

 

 

UPDATE 28/09/2015

 

Ok,

 

So I am getting more respose then I thought I would on this thread. I thought it would be a good idea to just explain exactly what I want to do.

 

I would like to control:

 

- LED Lights

- Power Outlets

- Main Lights

- Stereo & Speakers in different rooms (Like a sono)

- View security cameras

- +More

 

And I would like to control it all from a interface (That looks like Lcars (Massive Nerd)) that can be accessed from laptop, phone and main tablet.

 

What are your thoughts now?

 

UPDATE 03/10/2015


Ok, I have got all the parts and I have been able to control my LED strip via IR which I was over the moon about, I also connected it a python server and was able to control over the internet.

 

FYI I am using this guide: Controlling your stereo over the web with the Arduino infrared library

 

But now... The hardest part, how do I make this wifi? i have a esp8266 and would love to use it...

 

Or is my only option is to connect it to a pi running the server and have the PI wifi?

 

Let me know please.

 

Aiden

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    PHP has no bearing on a consistent URL As for how to do this, you can look at the Internet of Holiday Lights contest from Last winter, it has many examples of wireless and Internat controllable devices…
  • phoenixcomm
    phoenixcomm over 10 years ago in reply to scorpion +1
    no! use off the shelf remote controlled outlets!! That way you are National Electric Code safe!! look at https://www.nema.org/About/Join/Documents/NEMA%20Product%20Scopes.pdf these outlets have been around…
  • phoenixcomm
    phoenixcomm over 10 years ago +1
    for NEMA parts: https://www.vikingelectric.com/Images/img/043180/GE%20RS2-37.pdf
Parents
  • phoenixcomm
    0 phoenixcomm over 10 years ago

    for NEMA parts: https://www.vikingelectric.com/Images/img/043180/GE%20RS2-37.pdf

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to phoenixcomm

    There was a discussion in Forget Me Not using 433MHz RF controlled Mains outlets.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 10 years ago in reply to phoenixcomm

    There was a discussion in Forget Me Not using 433MHz RF controlled Mains outlets.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • phoenixcomm
    0 phoenixcomm over 10 years ago in reply to mcb1

    that last link was not the RF stuff its the GE low voltage stuff that I talked about.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to phoenixcomm

    GE low voltage stuff that I talked about.

    oops sorry I misunderstood.