Arduino Forum Having trouble switching a relay for my arduino project
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
  • State Not Answered
  • Replies 17 replies
  • Subscribers 392 subscribers
  • Views 1112 views
  • Users 0 members are here
  • arduino
  • relay
Related

Having trouble switching a relay for my arduino project

gub11
gub11 over 10 years ago

I am trying to switch this relay  https://www.sparkfun.com/products/10924  .  I don't think a schematic is necessary so i'll just explain it.  I have my that relay with GND to GND and the signal or vcc or whatever you want to call it pin hooked up to a digital out pin on the arduino, and the pin is writing high then low every 1 second, just to test it.  then i have a positive current running through the relay, that should be switched on and off with a one second delay powering an LED, but it isn't switching, it remains closed.  i have heard that it is because the arduino's digital write high voltage isn't enough to switch the relay, but i'm not sure because it was switching my 10A relay jsut fine.  Ideas?  I realize there is a datasheet but im still new to this kind of stuff so i don't really know what any of it means.

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 10 years ago +4
    Gabriel; They're trying to teach you how to find and interpret the information, so you can answer your own question. To read a schematic you need to know some of the common lingo, and how things are annotated…
  • shabaz
    shabaz over 10 years ago in reply to gub11 +3
    Gabriel, Please take the time to read it. I quickly scanned it, but it clearly indicated the transistor part number on the schematic, and even provided a URL to the part to help you. How do you expect…
  • shabaz
    shabaz over 10 years ago in reply to gub11 +1
    JP2 is not a transistor. You could have looked up 'transistor' in Wikipedia and identified the symbol if there was any confusion. At this point, I don't know what to suggest I'm afraid. I'm not prepared…
Parents
  • shabaz
    0 shabaz over 10 years ago

    Gabriel Spound wrote:

     

    but i'm not sure because it was switching my 10A relay jsut fine.

     

    I can't believe that - your 10A relay must have had additional circuitry on-board such as a transistor.

     

    The information you seek is in the comments on the sparkfun page that you refer to:

     

    (Quote:)

    Can you drive this directly from an Aruino?? It says power consumption is 0.9W @ 5.0V, that’s 180mA, which exceeds the current capability of an Arduino port.

    Rohar / about 2 years ago /  1

    You cannot drive it directly from an Arduino, but you can add a transistor to the circuit. The Arduino activates the transistor, the transistor activates the relay. See the Relay Tutorial to see exactly how this is accomplished.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gub11
    0 gub11 over 10 years ago in reply to shabaz

    the board that my 10a relay is on as a diode and a little black square with 2 contact points, sorry for being so vague  here it is   Keyes 5V Relay Module for Arduino (Works with Official Arduino Boards) - Free Shipping - DealExtreme

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gub11
    0 gub11 over 10 years ago in reply to shabaz

    the board that my 10a relay is on as a diode and a little black square with 2 contact points, sorry for being so vague  here it is   Keyes 5V Relay Module for Arduino (Works with Official Arduino Boards) - Free Shipping - DealExtreme