Arduino Forum Need some urgent help related to this Arduino Audio processing
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
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 392 subscribers
  • Views 817 views
  • Users 0 members are here
Related

Need some urgent help related to this Arduino Audio processing

Former Member
Former Member over 9 years ago

I am following this link from instructable site..

 

 

http://www.instructables.com/id/Arduino-Audio-Input/

 

My question is,

 

Instead of using the Microphone Radioshack 33-3038, which is listed in the tutorial , can I  use  https://www.sparkfun.com/products/9964,

 

KIndly suggest is there any modifications required in other parts for the circuitary If I go for Electret Microphone .

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +2 suggested
    Hi Raviraz, Yes there is a difference between the two microphones. The 33-3038 is a dynamic microphone which means that it is a coil of wire in a magnetic field. Sound waves vibrate the diaphragm and this…
  • Former Member
    Former Member over 9 years ago in reply to jw0752 +1
    Thanks once again John. I am pretty new bee in Arduino. My basic theme is to calculate the frequency of the sound generating from my test device",So i have chosen this instructble to help. I will try to…
Parents
  • jw0752
    0 jw0752 over 9 years ago

    Hi Raviraz,

    Yes there is a difference between the two microphones. The 33-3038 is a dynamic microphone which means that it is a coil of wire in a magnetic field. Sound waves vibrate the diaphragm and this moves the coil in the magnetic field and produces the electric signal. The Spark Fun microphone is an Electret condensor mic and it uses a different system involving a charged metal plate and a capacitive effect to convert the sound into an electric signal. The Electret also has a built in FET amplifier to amplify the electric signal to a usable level. I am sure that the Sparkfun mic will work but you will have to provide power to it from your board as it is has three wires Ground, Signal, and Power, whereas the Radio Shack Mic has only two wire Ground and Signal. Sparkfun usually has good documentation and they will likely include instruction to make the mic work with your project.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to jw0752

    Thank you so much John.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to jw0752

    Thank you so much John.