Arduino Forum Seeed Bluetooth Shield Issue
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
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 402 subscribers
  • Views 696 views
  • Users 0 members are here
  • bluetooth
  • arduino
Related

Seeed Bluetooth Shield Issue

wallarug
wallarug over 10 years ago

Hey all,

 

I'm having an issue with my Bluetooth shield set up, where if I connect everything up to my BoeBot Shield + the Bluetooth Shield, the Arduino crashes/restarts.  See below for more details.

 

Setup (on robot)

  • Arduino Uno
  • Boe-Bot Sheild (similar to: https://www.parallax.com/product/28832)
    • With two 360* full rotation servo motors
  • Seeedruino Bluetooth Shield (http://www.seeedstudio.com/wiki/Bluetooth_Shield)  --> Set up to run as a master.
  • HD44780 Character display (using a 74HC595 shift register to reduce the number of pins used)
  • HC-SR04 Distance Sensor

(separate)

  • Arduino Uno
  • Seeedruino Bluetooth Shield  --> Set up to run as a master

 

Issue / Behaviour:

  • Arduino is powered on > the sketch goes into the setup function > the setup() calls a bluetoothsetup() function.
  • The bluetooth fails to connect with it's paired shield.
  • COMMENT: Everything appears to work up to the delay(), where halfway through the delay(), the device crashes (BEFORE it gets to the loop() function.

 

When I run the below sample program, everything works as expected.  It is just when I try to use the Seeedruino Bluetooth in my custom code that it doesn't work.  I bought a HC-06 Bluetooth device, and that works fine with everything connected (HC-06 connects to laptop's bluetooth).

 

Everything is connected correctly.

 

Can anyone help point me in the right direction here?

Custom Code - uploaded to robot

/*

*  Written By: Cian Byrne 2015

*

*  Sensors Used:

*    - HC-SR04 Distance Sensor

HD47780 Character LCD Display(via  74HC595N74HC595N

*    - Servo Motor

*    - BoeBot Sheild

*/

 

 

#include <LiquidCrystal595.h>    // include the library

#include <SoftwareSerial.h>   //Software Serial Port

#include <Servo.h>

 

 

/*

* define global pins:

*/

#define trigPin 9

#define echoPin 6

#define servoPin 11

#define RxD 7

#define TxD 6

 

 

#define DEBUG_ENABLED 1

 

 

/*

* Variables

*/

int pos = 0;                                  //variable to store the servo position

long duration, distance;                      //variables to store the SR04 values

String slaveAddr = "0,6A,8E,16,C4,FD";        //MAC address of other BT sheild.

int distances[180];                           //Array to dump values from distance sensor

byte dataPacketA[180];                        //Array to dump values from distance sensor

 

 

SoftwareSerial blueToothSerial(RxD,TxD);

Servo ultraServo;                             // create servo object to control a servo

LiquidCrystal595 lcd(3,4,5);                  // datapin, latchpin, clockpin

 

 

 

 

/*

* Set up function

*/

void setup() {

  /*

   *  Serial set up (hardware and bluetooth

   */

  Serial.begin(9600);

  pinMode(RxD, INPUT);

  pinMode(TxD, OUTPUT);

  setupBlueToothConnection();

  //wait 1s and flush the serial and btooth buffers

  delay(1000);

  Serial.flush();

  blueToothSerial.flush();

 

  /*

   *  Servo and LCD Display

   */

 

  ultraServo.attach(servoPin);  // attaches the servo on pin 9 to the servo object

  ultraServo.write(90);   //set servo to middle position

 

  lcd.begin(16,2);         // 16 characters, 2 rows

  lcd.clear();

  lcd.setCursor(0,0);

 

 

  /*

   * SR HC-06 - Distance Sensor

   */

  pinMode(trigPin, OUTPUT);

  pinMode(echoPin, INPUT);

 

 

}

 

 

void loop() {

 

  // REMOVED CODE LOGIC

 

 

 

    //  send data over serial to PC:

    blueToothSerial.write(dataPacketA,180);

    Serial.write(dataPacketA,180);

}

 

 

 

// CODE REMOVED

 

 

 

 

 

/*

*  This is for the Seeedruino Bluetooth device

*/

void setupBlueToothConnection()

{

  // Set BluetoothBee BaudRate to default baud rate 38400

  blueToothSerial.begin(38400);

  // set the bluetooth work in master mode

  blueToothSerial.print("\r\n+STWMOD=1\r\n");

  // set the bluetooth name (irrelevant)

  blueToothSerial.print("\r\n+STNA=Master20\r\n");

  // Auto-connection is forbidden here

  blueToothSerial.print("\r\n+STAUTO=0\r\n");

  // This delay is required.

  delay(2000);

  blueToothSerial.flush();

  // This delay is required.

  delay(2000);

 

 

  //form the full connection command

  Serial.print("Connecting to slave: ");

  Serial.println(slaveAddr);

  //send connection command

  blueToothSerial.print("\r\n+CONN=" + slaveAddr + "\r\n");

  delay(5000);

}

 

 

/*

* This is for the HC-06 Bluetooth

*/

void setupBluetoothConn(){

  //Set BluetoothBee BaudRate to default baud rate 9600

  blueToothSerial.begin(9600);

  //delay

  delay(2000);

}

Sample Code (that works!) - uploaded to receiving Arduino connected to USB serial port

#include <SoftwareSerial.h>                     // Software Serial Port

 

 

#define RxD 7

#define TxD 6

 

 

#define DEBUG_ENABLED  1

 

 

// Make sure you modify this address to the one in your Slave Device!!

String slaveAddr = "0,6A,8E,16,C4,FD";

 

 

SoftwareSerial blueToothSerial(RxD,TxD);

 

 

void setup()

{

  Serial.begin(9600);

  pinMode(RxD, INPUT);

  pinMode(TxD, OUTPUT);

  setupBlueToothConnection();

  //wait 1s and flush the serial and btooth buffers

  delay(1000);

  Serial.flush();

  blueToothSerial.flush();

}

 

 

void loop()

{

  char recvChar;

 

 

  // Infinite loop

  while(1)

  {

    // If there is data pending to be read from the shield

    if(blueToothSerial.available())

    {

      recvChar = blueToothSerial.read();

      // Print the data through the Serial channel

      Serial.print("Master Received: ");

      Serial.print(recvChar);

      Serial.print("\n");

    }

    // If there is data pending to be read from the serial port

    if(Serial.available())

    {

      recvChar  = Serial.read();

      // Send the data through btooth

      blueToothSerial.print(recvChar);

      Serial.print("Master Transmitted: ");

      Serial.print(recvChar);

      Serial.print("\n");

    }

  }

}

 

 

// Function to start the connection. Make sure slaveAddr is set to the right

// value.

void setupBlueToothConnection()

{

  // Set BluetoothBee BaudRate to default baud rate 38400

  blueToothSerial.begin(38400);

  // set the bluetooth work in master mode

  blueToothSerial.print("\r\n+STWMOD=1\r\n");

  // set the bluetooth name (irrelevant)

  blueToothSerial.print("\r\n+STNA=Master20\r\n");

  // Auto-connection is forbidden here

  blueToothSerial.print("\r\n+STAUTO=0\r\n");

  // This delay is required.

  delay(2000);

  blueToothSerial.flush();

  // This delay is required.

  delay(2000);

 

 

  //form the full connection command

  Serial.print("Connecting to slave: ");

  Serial.println(slaveAddr);

  //send connection command

  blueToothSerial.print("\r\n+CONN=" + slaveAddr + "\r\n");

  delay(5000);

}

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago +1 suggested
    wallarug wrote: Custom Code - uploaded to robot /* * define global pins: */ #define trigPin 9 #define echoPin 6 #define servoPin 11 #define RxD 7 #define TxD 6 You appear…
  • gadget.iom
    gadget.iom over 10 years ago in reply to wallarug +1
    Glad you're all sorted. Paul
Parents
  • gadget.iom
    0 gadget.iom over 10 years ago

    Can you try using the shields one at at time and see if the bluetooth shield will work on the UNO on its own?

    You may be having an issue with power, or a pin conflict between two shields.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 10 years ago

    Can you try using the shields one at at time and see if the bluetooth shield will work on the UNO on its own?

    You may be having an issue with power, or a pin conflict between two shields.