Arduino
  • Products
  • More
Arduino
Arduino Forum Motors for Arduino and embedded PC projects
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 854 views
  • Users 0 members are here
  • motor
  • arduino
Related

Motors for Arduino and embedded PC projects

amrrahmy
amrrahmy over 10 years ago

I have read a bit about the differences between DC / servo / stepper motors, but I would like to know more before delving any deeper.

 

the projects will use

  • Arduino Uno (possibly Arduino Zero in the future or other ARM micro-controllers),
  • 5.3V 2A USB smartphone charger as the input

 

wanted to make a "pan / tilt"(possibly 360 degree) platform for a solar panel (3W or 5W + the weight or the platform (probably made of wood))

  • are there any pros or cons if I use a servo vs stepper motor(more components, more expensive, more power required, more accuracy)

 

wanted to make a lift(elevator) and pulley system that would lift and move maybe 1-2KG(2-4 pounds) across 1 meter distance(might add hydraulics if needed)

  • would a DC motor have more torque if I added gears or would I be better off looking for a servo motor(any additional electronics needed for either? transformers, more power required to do the same job, ...etc.)
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago in reply to amrrahmy +2 suggested
    Hi Amr, You can connect the hobby servo to an external supply yes, and connect the control wire to a digital output on the Arduino (a pulse width modulation or PWM signal is used, see here ). Motor drivers…
  • shabaz
    shabaz over 10 years ago +1 verified
    Hi Amr, There is a post here that highlights some differences between the various types of motors . There are example photos there too, so you can recognise the motors. A 3W/5W panel is fairly small, so…
Parents
  • shabaz
    0 shabaz over 10 years ago

    Hi Amr,

     

    There is a post here that highlights some differences between the various types of motors. There are example photos there too, so you can recognise the motors.

    A 3W/5W panel is fairly small, so you could possibly use a hobby servo, I don't think you need much accuracy. If you use a stepper or some other motor then you need a driver circuit; you won't need that with a hobby servo.

    For a suitable circuit for brushed motors, consider the infineon DC motor driver board. It is overkill if you just want to drive a very small motor though. (Also I think most cheap motors are not brushless by the way).

    Virtually any motor can lift 2-4 pounds, as long as it is geared down heavily enough (but then will take time performing the motion of course).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • amrrahmy
    0 amrrahmy over 10 years ago in reply to shabaz

    Thank you for the quick reply,

     

    I have settled on the 2 servo for the pan / tilt panel. I can plug the servo into external power source and plug analog wire into the Arduino, right? it would not need to take power from the Arduino?

     

    I am still confused about

    • motor drivers and driver shields (this is for higher voltage devices?)
    • transformers and mosfets (I think its for controlling a higher voltage circuit using a lower voltage circuit)
    • ESC for brush-less motors (this is for higher current devices?)
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to amrrahmy

    Hi Amr,

     

    You can connect the hobby servo to an external supply yes, and connect the control wire to a digital output on the Arduino (a pulse width modulation or PWM signal is used, see here).

    Motor drivers are for controlling a power source (e.g. battery) to drive a motor, based on control from the Arduino. They are needed because motors use far higher power that the digital outputs available from the Arduino. The analog signal is not used - it is easier to rapidly pulse the digital signal to control speed based on PWM.

    Transformers or MOSFETs are used to construct motor drivers, but it is harder than just buying a motor driver board. (The Infineon board blog post describes what the internals look like using MOSFETs in a

    'Half-Bridge' or 'H-bridge' representation , but it is just a high level diagram. Beware there are plenty of bad circuits circulating on the Internet that attempt to construct motor driver boards from discrete semiconductors).

    For brushless motors a different circuit is needed, sometimes known as an ESC. Like any other motor, brushless motors use higher power than the Arduino outputs are capable of.

    Again, transistors or MOSFETs (technically a MOSFET is a transistor by the way - just by 'transistor' alone people usually mean a 'Bipolar Junction Transistor' or BJT) are used to construct this circuit too.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 10 years ago in reply to amrrahmy

    Hi Amr,

     

    You can connect the hobby servo to an external supply yes, and connect the control wire to a digital output on the Arduino (a pulse width modulation or PWM signal is used, see here).

    Motor drivers are for controlling a power source (e.g. battery) to drive a motor, based on control from the Arduino. They are needed because motors use far higher power that the digital outputs available from the Arduino. The analog signal is not used - it is easier to rapidly pulse the digital signal to control speed based on PWM.

    Transformers or MOSFETs are used to construct motor drivers, but it is harder than just buying a motor driver board. (The Infineon board blog post describes what the internals look like using MOSFETs in a

    'Half-Bridge' or 'H-bridge' representation , but it is just a high level diagram. Beware there are plenty of bad circuits circulating on the Internet that attempt to construct motor driver boards from discrete semiconductors).

    For brushless motors a different circuit is needed, sometimes known as an ESC. Like any other motor, brushless motors use higher power than the Arduino outputs are capable of.

    Again, transistors or MOSFETs (technically a MOSFET is a transistor by the way - just by 'transistor' alone people usually mean a 'Bipolar Junction Transistor' or BJT) are used to construct this circuit too.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer