Arduino Forum Arduino internal clock inaccurate??
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
  • State Verified Answer
  • Replies 14 replies
  • Subscribers 402 subscribers
  • Views 1134 views
  • Users 0 members are here
  • clock
  • explodedclock
  • brass
  • collectable
  • antique
  • art
  • arduino
  • no4
Related

Arduino internal clock inaccurate??

jonivanart
jonivanart over 10 years ago

Hello! I am a newbie here and fairly new with the Arduino. I am building a piece of art that has a 150 year old clock as the main subject. I am going to use an Arduino to drive a stepper that runs the clock, a DC motor for the Chime drive (For visual effect) and a solenoid for the escapement mechanism also for visual effect. I've heard that the internal clock on the Arduino is inaccurate from others. What will I need to make it have an accurate output?image

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +3 verified
    Hi Jon, Interesting project! Will it not damage the mechanism though? Maybe something like that is worth a lot of money. You didn't say how accurate you wanted : ) Anyway, the Arduino clock is ok, but…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    It sounds like what you need is a very accurate pulse / time period, not he arduino actually keeping time Using an internet connected NTP client as sugested by shabaz would be an easy way to keep time…
  • jonivanart
    jonivanart over 10 years ago in reply to shabaz +1
    Thanks! To answer the first question. "Will it damage the clock and maybe it's worth a lot of money? I have plans to put the drive on the proper gear with the least amount of drag/pressure on the coupling…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    It sounds like what you need is a very accurate pulse / time period, not he arduino actually keeping time

     

    Using an internet connected NTP client as sugested by shabaz would be an easy way to keep time with the arduino and will allow for drift over time to be corrected based on how often you re-synce with the NTP server, but between syncs it will drify a little

     

    What I think you really need though is a very precise pulse being sent to the stepper or solenoid, if you count the pulses or steps being sent and compare to the actual time after each NTP server sync, if too many pulses have been sent you can slow down ever so slightly, if too many then speed up a small amount, this way, the clock may be out from time to time but should correct it self automatically

     

    At least theory sounds right image

     

    Good luck

    Peter

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    It sounds like what you need is a very accurate pulse / time period, not he arduino actually keeping time

     

    Using an internet connected NTP client as sugested by shabaz would be an easy way to keep time with the arduino and will allow for drift over time to be corrected based on how often you re-synce with the NTP server, but between syncs it will drify a little

     

    What I think you really need though is a very precise pulse being sent to the stepper or solenoid, if you count the pulses or steps being sent and compare to the actual time after each NTP server sync, if too many pulses have been sent you can slow down ever so slightly, if too many then speed up a small amount, this way, the clock may be out from time to time but should correct it self automatically

     

    At least theory sounds right image

     

    Good luck

    Peter

    • Cancel
    • Vote Up +2 Vote Down