Arduino
  • Products
  • More
Arduino
Arduino Forum Can't understand how the program is working
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 1114 views
  • Users 0 members are here
Related

Can't understand how the program is working

e14 Contributor
e14 Contributor over 10 years ago

How does the Serial monitor display '12594' when we write Serial.print('12');?I have used single quotes intentionally.

[code]

void setup()

{

Serial.begin(9600);

Serial.print('12');

}


void loop()

{

}

[/code]

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago in reply to e14 Contributor +1 suggested
    Single quotes are typically used to declare character constants (that means only on character is permitted within the quotes). The compiler should give you warning if you try to include more than one character…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1 verified
    when you output '12' your outputting 2 characters, a '1' and then a '2', this results in hex 31 or dec 49 being transmitted followed by a 32hex / 50dec, if you concatinate the two into a single integer…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to gadget.iom +1
    according to C99 this is implementation specefic so for the Arduino compiler it apears to be interpreting the character literal as an int which is perfectly valid go figure
Parents
  • gadget.iom
    0 gadget.iom over 10 years ago

    Why are you using single quotes?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to gadget.iom

    If we write Serial.print('6'); then its ASCII value get printed.I wanted to see what happens when we write Serial.print('12');.........You may even try Serial.print('10'); or Serial.print('11');

    The values in that case comes out t o be '12592' and '12593' respectively.So I want to know what is actually happening

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to e14 Contributor

    Single quotes are typically used to declare character constants (that means only on character is permitted within the quotes).

    The compiler should give you warning if you try to include more than one character.

     

    sketch_dec17a.ino:4:14: warning: multi-character character constant [-Wmultichar]

     

    In practice, what you are seeing is down to either of the following:

    The value of 'ab' is likely to be either 'a' * 256 + 'b'

    or 'b' * 256 + 'a'. It will vary from one compiler to another.

    In his case (where ASCII 1=49 and ASCII 2=50 you are likely seeing:

     

    (49*256)+50 = 12594

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to gadget.iom

    according to C99 this is implementation specefic so for the Arduino compiler it apears to be interpreting the character literal as an int which is perfectly valid

     

    go figure

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to gadget.iom

    according to C99 this is implementation specefic so for the Arduino compiler it apears to be interpreting the character literal as an int which is perfectly valid

     

    go figure