Arduino
  • Products
  • More
Arduino
Arduino Forum Using a Garmin Nuvi as a display?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 417 subscribers
  • Views 3620 views
  • Users 0 members are here
  • display
  • gps
  • arduino
  • garmin
Related

Using a Garmin Nuvi as a display?

rx7man
rx7man over 10 years ago

I was thinking... There's lots of old GPS systems available now for cheap.. even new ones are cheap.. to the point they're cheaper than buying the components to make a display.

 

I picked up a Nuvi 265W, it has bluetooth, and is powered with a Garmin branded STmicro chip, and a 2gb samsung memory chip as well

 

What I was really wondering is if there's any way to interface this with an arduino... Using the display to show graphs and/or text relating to the state of variables, inputs, and outputs on the Arduino... perhaps access the GPS data (not my primary goal), and perhaps even using bluetooth as a COM port to transfer data to a smartphone?  There's tons of possibilities, I'm wondering if it's ever been done?

 

My current Arduino platforms are the Mega 2560, Uno, and Leonardo

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 10 years ago

    Here is a long shot (low probability of working) you could look into:

    - See if the GPS can play a slideshow from an SD card (I think my Garmin can),

    - use an Eyefi or SD/USB card to load new pictures into the SD card while it is plugged into the GPS

    - If you can delete old pictures and only have one image in the directory, maybe the GPS will display the latest update.

    I suspect this cannot be done on the fly, but maybe you can get updates without too many refresh steps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 10 years ago

    Here is a long shot (low probability of working) you could look into:

    - See if the GPS can play a slideshow from an SD card (I think my Garmin can),

    - use an Eyefi or SD/USB card to load new pictures into the SD card while it is plugged into the GPS

    - If you can delete old pictures and only have one image in the directory, maybe the GPS will display the latest update.

    I suspect this cannot be done on the fly, but maybe you can get updates without too many refresh steps.