Arduino
  • Products
  • More
Arduino
Arduino Forum Using a Garmin Nuvi as a display?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 417 subscribers
  • Views 3605 views
  • Users 0 members are here
  • display
  • gps
  • arduino
  • garmin
Related

Using a Garmin Nuvi as a display?

rx7man
rx7man over 10 years ago

I was thinking... There's lots of old GPS systems available now for cheap.. even new ones are cheap.. to the point they're cheaper than buying the components to make a display.

 

I picked up a Nuvi 265W, it has bluetooth, and is powered with a Garmin branded STmicro chip, and a 2gb samsung memory chip as well

 

What I was really wondering is if there's any way to interface this with an arduino... Using the display to show graphs and/or text relating to the state of variables, inputs, and outputs on the Arduino... perhaps access the GPS data (not my primary goal), and perhaps even using bluetooth as a COM port to transfer data to a smartphone?  There's tons of possibilities, I'm wondering if it's ever been done?

 

My current Arduino platforms are the Mega 2560, Uno, and Leonardo

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Hello Efrem,

     

    I think that this imply to hack in some way the GPS but the concept sounds very good. The first problem is from where do you want to access to the device from the Arduino. And for this decision it is needed to have some documentation on what it is possible to do or not to do with the available peripheral first and in second instance disassemble the system and check in detail the circuit to see if it is possible to understand how it works.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Hello Efrem,

     

    I think that this imply to hack in some way the GPS but the concept sounds very good. The first problem is from where do you want to access to the device from the Arduino. And for this decision it is needed to have some documentation on what it is possible to do or not to do with the available peripheral first and in second instance disassemble the system and check in detail the circuit to see if it is possible to understand how it works.

     

    Enrico