Arduino Forum Pin interference
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
  • State Not Answered
  • Replies 6 replies
  • Subscribers 393 subscribers
  • Views 511 views
  • Users 0 members are here
  • ham
  • help
  • diy
  • arduino
Related

Pin interference

Former Member
Former Member over 9 years ago

Hi,
New to this forum so I hope this is the correct place to ask for help.
I have searched, both inside and outside of this forum but can't find anything to help me.

 

 

My setup is located in my car

My problem is that I have a HAM-radio close to the arduino ( about 50cm) and when I set the radio to transmit at >30W, one or more pins on the arduino goes high and triggering my system.

I have a pulldown resistor at 10K on each pin but that doesn't help.

Is there a way for me to shield the arduino from this interference?

The systems share a 12V-line but have there own grounds to the battery.

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    0 mcb1 over 9 years ago

    one or more pins on the arduino goes high and triggering my system.

    Do you know if the pins are used within the program.?

     

    As jw0752 has suggested I suspect you might be getting spikes up the 12v line.

    Arduino have some filtering but in reality it is minimal and since a vehicle delivers 14.2v when running, it is operating at the limits of the regulator.

    For my automotive application I used an 8v regulator prior to the on-board 5v, and you could apply filtering there.

     

    A simple check could be powering the Arduino from another source.

     

    The inputs on Arduino are very high impedance, so your precaution of pulling down the inputs with a 10k is good, but your external connections may be picking enough RF to overcome this.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 9 years ago

    one or more pins on the arduino goes high and triggering my system.

    Do you know if the pins are used within the program.?

     

    As jw0752 has suggested I suspect you might be getting spikes up the 12v line.

    Arduino have some filtering but in reality it is minimal and since a vehicle delivers 14.2v when running, it is operating at the limits of the regulator.

    For my automotive application I used an 8v regulator prior to the on-board 5v, and you could apply filtering there.

     

    A simple check could be powering the Arduino from another source.

     

    The inputs on Arduino are very high impedance, so your precaution of pulling down the inputs with a 10k is good, but your external connections may be picking enough RF to overcome this.

     

    Mark