Arduino
  • Products
  • More
Arduino
Arduino Forum HOW TO DRIVE A PIEZODEVICE
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 419 subscribers
  • Views 1577 views
  • Users 0 members are here
Related

HOW TO DRIVE A PIEZODEVICE

e14 Contributor
e14 Contributor over 10 years ago

I used to be knowledgable in these things but I have had some health problems (stroke and heart attack)  which have left me with some  blank spots in my memory.

 

So I would appreciate some help on some things.

 

I want to drive a piezo device at about 50 or 60 Hz.  This will create a ping or beep.

I want it to pulse for a predetermined time each time I press a button.

Do I need current limiting resistors or driver transistor?

 

Is there any one who can help me with this?

 

bob

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 10 years ago +2
    Hi Bob, Depending on how loud you need the sound to be you could conceivably drive the piezo directly off a 555 timer. There are also little piezo buzzers with a built in oscillator that could be incorporated…
  • michaelkellett
    michaelkellett over 10 years ago in reply to jonivanart +1
    Sorry Jon, I was replying to Bob when he said: I have seen on the internet if you put a piezo device in a small plastic container filled with mineral oil it will work as a transducer able to send out a…
  • clem57
    clem57 over 10 years ago +1
    Why not use sonar? C
Parents
  • jw0752
    0 jw0752 over 10 years ago

    Hi Bob,

    Depending on how loud you need the sound to be you could conceivably drive the piezo directly off a 555 timer. There are also little piezo buzzers with a built in oscillator that could be incorporated in an even simpler circuit. Give me a little more information on your requirements and what parts you already have and I will draw up a suggested circuit. you suggest a frequency of 50 or 60 Hz but this is quite low and would be more like a hum as oppose to a beep or a ping.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jw0752

    End result I want to make a unit that will measure distance underwater. 

    It has to be omnidirectional.  Transducers for depth finders and fish

    locators are somewhat directional in a 60 deg. cone.  I have seen on the

    internet if you put a piezo device in a small plastic container filled

    with mineral oil it will work as a transducer able to send out a ping. 

    Then you are set.

     

    I want to use a Arduino to control the device.

     

    Bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 10 years ago in reply to e14 Contributor

    Hi Bob,

    Thanks for the additional information. The complexity of what you describe is above my expertise. I am also confused about what you mean by an omni-directional distance measuring device. Such a device would need to return a three dimensional surface that is representative of the distance to objects in all directions. Also there would still be granulation as the resolution would have to be limited. Perhaps it would be easier to build a device like the fish sonar and then use it to sweep and return directional data. You could then integrate the directional data to yield a more complete picture. Once again I apologize for not being able to help further on this project. I hope you are able to find someone with more knowledge to assist.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 10 years ago in reply to e14 Contributor

    Just a small addendum. Your specified frequency of 50 to 60 cycles would yield very low resolution data but it would have a greater distance of penetration. Higher frequency sound would give much better resolution but at the cost of distance.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 10 years ago in reply to e14 Contributor

    Just a small addendum. Your specified frequency of 50 to 60 cycles would yield very low resolution data but it would have a greater distance of penetration. Higher frequency sound would give much better resolution but at the cost of distance.

    John