Arduino Forum Programming The Atmega2560 with Arduino
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
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 403 subscribers
  • Views 1656 views
  • Users 0 members are here
  • arduino_tutorials
  • arduino_tutorial
Related

Programming The Atmega2560 with Arduino

technocat
technocat over 9 years ago

Hi everyone,

 

I joined element14 because I recently started building a PCB on Eagle for an independent study for school, and I need some help.

 

I want to use the Atmega2560 board due to its large analog input, digital I/O capacity, and Arduino uses it in the Mega so the pinouts are simple. My only issue is that I can't find a way to program the board!

 

It seems that the Atmega2560 doesn't come with the Arduino bootloader installed (not surprising) and I can't find a pre-bootloaded board on the internet either, like some other Atmel boards.

 

My question really is:

 

How can I upload an Arduino sketch a stock Atmel ATMega2560 IC?

 

Thanks A LOT to anyone with information!

  • Sign in to reply
  • Cancel

Top Replies

  • technocat
    technocat over 9 years ago in reply to clem57 +2
    Hi Clem, I'm building a 10.5 foot drone that can take off vertically and fly horizontally. Its like the Osprey V-22. The hardware necessary to make that happen doesn't really exist beyond the commercial…
Parents
  • clem57
    0 clem57 over 9 years ago

    Interested to see what project you have in mind or this. Ty.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago

    Interested to see what project you have in mind or this. Ty.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • technocat
    0 technocat over 9 years ago in reply to clem57

    Hi Clem,

     

    I'm building a 10.5 foot drone that can take off vertically and fly horizontally. Its like the Osprey V-22.

     

    The hardware necessary to make that happen doesn't really exist beyond the commercial/military realm, so like most things I'm doing it myself.

     

    image

     

    With 3 motors, 4 vector related servos... I need at least 15 I/O pins to have full functionality, but I'm really for the upwards of around 25 I/O for servos because of cooling fans, opening/closing air vents, etc. Then there are lights, camera switchers... etc. Lots of I/O.

     

    The "motherboard" of the flight deck *I'm hoping* will be the ATMega2560 because of its large I/O capability, analog input count, and it seems the community is large enough with the chip. I'm designing it in Eagle CAD and will have it manufactured... somewhere. (Any recommendations...?)

     

    The difficult part will be the stabilization script while hovering, but right now it's based on PID control. I'm building the airframe concurrently with the circuitry, and hot damn it is fun!

    • Cancel
    • Vote Up +2 Vote Down