Arduino Forum Road speed limit project
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 392 subscribers
  • Views 519 views
  • Users 0 members are here
Related

Road speed limit project

Former Member
Former Member over 9 years ago

Hello, I'ts my first post here, so dont get mad if it's not the right subforum for this topic. I would just like some ideas/opinions for my project, because maybe I am forgetting something in addition to i am new with arduino

 

the idea is a device that tracks a car's speeds and omits a message to the driving control authority, in case the car exceeds the speed limit. so What I am trying to build, is a Speed limit notification system that can sense my location and speed using GPS then compare it to defined speed for the current road using algorithm then send data over GSM network to my webserver or mobile phone warning me if i exceed the speed limit .

 

What I need to achieve (and my plans to do so) are:

 

1. Arduino Uno

 

2. GPS module

http://www.zeroohm.ae/Adafruit-Ultimate ... search=gps


3. GSM shield for network connection or sms sending

 

http://www.zeroohm.ae/Arduino-GSM-Shiel ... search=gsm


5. so i will defined maybe two or three roads using this techniques and define any speed i want

http://forum.arduino.cc/index.php?topic=136265.0



Is these parts good ?

is it ok to connect GPS module through gsm shield to Arduino ?

I'm working on this project alone, maybe I have missed something, maybe theres a better solution for something, maybe someone else has some great ideas they are willing to share, regarding this idea and how to pull it off.

 

Thanks all

and sorry about my english

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago +1
    Hi Mohammad, There are hundreds of different GPS and GSM modules, but in general it doesn't matter what you use provided you have sufficient information (datasheets primarily) to get you going. If there…
Parents
  • Former Member
    0 Former Member over 9 years ago

    I'll echo the same thing shabaz mentioned about documentation.  You might also think about one of the shields that integrates GPS and GPRS on a single PCB.  There are a variety of distributors around the world that carry these.  These are largely intended to work with mobile robots, so if this interests you might want to look at those sites.

     

    As far as GPS and GSM/GPRS on the same PCB this isn't a problem.  GPRS signals are 850-900MHz and 1800-1900MHz.  GPS uses 1176.45, 1227.60, and 1575.42MHz; with code carriers down in the 4-10MHz regions.  There is enough difference in freqs used and carrier wave types that this isn't a problem (obvious, since most smartphones also have GPS built-in).  The only thing I might suggest is to use external antennas, if possible.  GPS signals can be degraded quite a bit, if a chip antenna is blocked.

     

    It's a cool idea!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago

    I'll echo the same thing shabaz mentioned about documentation.  You might also think about one of the shields that integrates GPS and GPRS on a single PCB.  There are a variety of distributors around the world that carry these.  These are largely intended to work with mobile robots, so if this interests you might want to look at those sites.

     

    As far as GPS and GSM/GPRS on the same PCB this isn't a problem.  GPRS signals are 850-900MHz and 1800-1900MHz.  GPS uses 1176.45, 1227.60, and 1575.42MHz; with code carriers down in the 4-10MHz regions.  There is enough difference in freqs used and carrier wave types that this isn't a problem (obvious, since most smartphones also have GPS built-in).  The only thing I might suggest is to use external antennas, if possible.  GPS signals can be degraded quite a bit, if a chip antenna is blocked.

     

    It's a cool idea!