Arduino
  • Products
  • More
Arduino
Arduino Forum Parsing integer strings?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 2 answers
  • Subscribers 410 subscribers
  • Views 2763 views
  • Users 0 members are here
  • serial_communications
  • potentiometers
  • parsing
  • boolean
  • arduino
Related

Parsing integer strings?

scorpion
scorpion over 10 years ago

I need help with parsing a string of integers sent from another Arduino. The values will be like this 1, 0, 1234, 1234,

1 is a Boolean

0 is a Boolean

1234 are pot values

I would like for it to go to variables

Vpot is first pot value

Hpot is second pot value

C is first Boolean

Z is second Boolean

 

Thanks,

Ben Bonen

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +1
    sscanf is your friend, probably supported by Arduino (I don't use Arduino). Reddit on the topic however is here. https://www.reddit.com/r/arduino/comments/pznnj/using_sscanf_with_arduino/
  • gadget.iom
    gadget.iom over 10 years ago +1
    The Serial.readStringUntil command may help you if you are receiving the data through the serial port. Something like this might work: void loop(){ String C = Serial.readStringUntil(',').toInt(); Serial…
  • clem57
    clem57 over 10 years ago +1
    One way is using indexOf( ) like in http://stackoverflow.com/questions/11068450/arduino-c-language-parsing-string-with-delimiter-input-through-serial-interf… Then easy to convert to known values. Suggest…
Parents
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Hi Ben,

     

    please find below the method I have used in several string parsers with the Arduino boards. This will work for sure.

     

    Enrico

     

    /** \fn int charsToInt(int startChar, int numChars)
        \brief Convert a string from the command to integer
    
    
        \param startChar initial character in the command string
        \param numChars number of characters composing the number
        \return The converted interger value
    */
    int charsToInt(int startChar, int numChars)
    {
        char * value_to_convert;
        String temp = String(6);
        int i;
    
    
        for (i = 0; i < numChars; i++)
            temp += cmd.cmdData[i + startChar];
    
    
        value_to_convert = temp;
        i = atoi(temp);
    
    
        return i;
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • scorpion
    0 scorpion over 10 years ago in reply to balearicdynamics

    @Enrico Miglino

    Thanks!

    Will this send the values to different variables?

    Ben

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • scorpion
    0 scorpion over 10 years ago in reply to balearicdynamics

    @Enrico Miglino

    Thanks!

    Will this send the values to different variables?

    Ben

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to scorpion

    Hi Ben,

     

    as this is an independent function, you can call it passing the string you want to parse and use the integer return value as well. About the error correction it is true, there is no error checking and - by my point of view - there is a reason. As this function is used in a parser; I mean, a string parser processing multiple kind of commands with or without parameters, command separators etc. when the conversion is called all the syntax check are already done.

     

    In your case I suggest you check before that the string you send is a valid numeric string that - by a pragmatic point of view - is something independent by the conversion function. In this moment I don't remember what kind of result aoti() call returns when a non-numeric character is passed.

     

    Enrico