Arduino
  • Products
  • More
Arduino
Arduino Forum Parsing integer strings?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 2 answers
  • Subscribers 410 subscribers
  • Views 2765 views
  • Users 0 members are here
  • serial_communications
  • potentiometers
  • parsing
  • boolean
  • arduino
Related

Parsing integer strings?

scorpion
scorpion over 10 years ago

I need help with parsing a string of integers sent from another Arduino. The values will be like this 1, 0, 1234, 1234,

1 is a Boolean

0 is a Boolean

1234 are pot values

I would like for it to go to variables

Vpot is first pot value

Hpot is second pot value

C is first Boolean

Z is second Boolean

 

Thanks,

Ben Bonen

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +1
    sscanf is your friend, probably supported by Arduino (I don't use Arduino). Reddit on the topic however is here. https://www.reddit.com/r/arduino/comments/pznnj/using_sscanf_with_arduino/
  • gadget.iom
    gadget.iom over 10 years ago +1
    The Serial.readStringUntil command may help you if you are receiving the data through the serial port. Something like this might work: void loop(){ String C = Serial.readStringUntil(',').toInt(); Serial…
  • clem57
    clem57 over 10 years ago +1
    One way is using indexOf( ) like in http://stackoverflow.com/questions/11068450/arduino-c-language-parsing-string-with-delimiter-input-through-serial-interf… Then easy to convert to known values. Suggest…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    This topic is fully covered in a seriese I posted a while back

     

    Fast Track to Arduino Programming

     

    Lesson 2 and 3 are the ones most relevent to your issue

     

    they use a C command strtok that allows parsing of strings using a provided token or tokens and is very powerful and perfect for this kind of scenario

     

    Enjoy

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    This topic is fully covered in a seriese I posted a while back

     

    Fast Track to Arduino Programming

     

    Lesson 2 and 3 are the ones most relevent to your issue

     

    they use a C command strtok that allows parsing of strings using a provided token or tokens and is very powerful and perfect for this kind of scenario

     

    Enjoy