Arduino Forum Arduino relay board distance limitations
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
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 403 subscribers
  • Views 946 views
  • Users 0 members are here
  • arduino
Related

Arduino relay board distance limitations

Former Member
Former Member over 9 years ago

I'm completely new to Arduino, but diving in head first. I presently have multiple isolated control boxes of timers and relays controlling a number of things around my home and hobby farm such as outdoor lighting at dusk, automatic feeding of horses 4 times a day, exhaust fans, opening and closing windows in the barn depending on temp and humidity. Well I think it's time I consolidated all these isolated devices into one controller and get with the times...... My first question is the operating distance a relay module can safely operate over 22 ga twisted pair wire. As I am bringing everything back to a central point in my home, my analog experience tells me to calculate voltage drop. I can remotely power each relay board, but the high/low digital signal is where I get lost. I don't know the current, and not sure if it's even relative with a digital signal. So...... I would appreciate any knowledge you can share with me regarding the maximum distance over 22ga twisted pair you can safely operate a relay module. I have one location of a pump, that is 900m away, will it work???? Can this be compared to DSL internet where the modem can be 7 or 8 km's from the exchange equipment and the digital signal is fine????

 

 

Love to hear your comments on this and any experience you've had.

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 9 years ago +2 suggested
    My first question is the operating distance a relay module can safely operate over 22 ga twisted pair wire The answer to that depends on the current required to operate the relay coil. Obviously the more…
  • Former Member
    Former Member over 9 years ago +1 suggested
    Hi I wouldn't opt for either of these two methods although they may work when you running fairly long distances I would personally consider using RS485 as the protocol to communicate btw smaller devices…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    I would suggest that you dont try to consolidate all the actual physical control points at the house but instead keep the switches / Reslays at the point of control. Upgrade them for sure to use Arduino, ESP8266 or other modules more suited to automated and modern control systems

     

    Have a House placed master controller for sure, running on a Raspberry PI 2 with 7" LCD would be awsome

     

    The control points though especially given 900M dstance would be better communicated with using either CAT3 or 5 twisted pair ethernet or RS485 serial communications, both of which are good for this distance (There up to 1200M or more)

     

    even WIFI is only typically good for about 300M with no obstructions though a sub Ghz radio link may easily cover the distance, for instance the TI sub GHz radio modules or many other types you can find arround the EBays and AlliExpresses of the world

     

    If you can provide a sketch of you proposed control system, (A Map of the farm so to speak) showing distances and the types of things your controlling, then I will be in a much better position to help

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    I would suggest that you dont try to consolidate all the actual physical control points at the house but instead keep the switches / Reslays at the point of control. Upgrade them for sure to use Arduino, ESP8266 or other modules more suited to automated and modern control systems

     

    Have a House placed master controller for sure, running on a Raspberry PI 2 with 7" LCD would be awsome

     

    The control points though especially given 900M dstance would be better communicated with using either CAT3 or 5 twisted pair ethernet or RS485 serial communications, both of which are good for this distance (There up to 1200M or more)

     

    even WIFI is only typically good for about 300M with no obstructions though a sub Ghz radio link may easily cover the distance, for instance the TI sub GHz radio modules or many other types you can find arround the EBays and AlliExpresses of the world

     

    If you can provide a sketch of you proposed control system, (A Map of the farm so to speak) showing distances and the types of things your controlling, then I will be in a much better position to help