Arduino Forum Arduino relay board distance limitations
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
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 403 subscribers
  • Views 947 views
  • Users 0 members are here
  • arduino
Related

Arduino relay board distance limitations

Former Member
Former Member over 9 years ago

I'm completely new to Arduino, but diving in head first. I presently have multiple isolated control boxes of timers and relays controlling a number of things around my home and hobby farm such as outdoor lighting at dusk, automatic feeding of horses 4 times a day, exhaust fans, opening and closing windows in the barn depending on temp and humidity. Well I think it's time I consolidated all these isolated devices into one controller and get with the times...... My first question is the operating distance a relay module can safely operate over 22 ga twisted pair wire. As I am bringing everything back to a central point in my home, my analog experience tells me to calculate voltage drop. I can remotely power each relay board, but the high/low digital signal is where I get lost. I don't know the current, and not sure if it's even relative with a digital signal. So...... I would appreciate any knowledge you can share with me regarding the maximum distance over 22ga twisted pair you can safely operate a relay module. I have one location of a pump, that is 900m away, will it work???? Can this be compared to DSL internet where the modem can be 7 or 8 km's from the exchange equipment and the digital signal is fine????

 

 

Love to hear your comments on this and any experience you've had.

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 9 years ago +2 suggested
    My first question is the operating distance a relay module can safely operate over 22 ga twisted pair wire The answer to that depends on the current required to operate the relay coil. Obviously the more…
  • Former Member
    Former Member over 9 years ago +1 suggested
    Hi I wouldn't opt for either of these two methods although they may work when you running fairly long distances I would personally consider using RS485 as the protocol to communicate btw smaller devices…
Parents
  • mcb1
    0 mcb1 over 9 years ago

    My first question is the operating distance a relay module can safely operate over 22 ga twisted pair wire

    The answer to that depends on the current required to operate the relay coil.

    Obviously the more powerful the relay, the larger the coil.

     

    You could trigger an optocoupler, which then operates the relay on the board.

    It seems you can provide power to the board, but the control wire size is limited.

     

    To give an idea, I have some trip systems at the skifield that are 1km away from the switch.

    Bascally 5v is fed into Pin1 (Anode) of an optocoupler, and Pin 2 (Cathode) travels 1km up the wire, then the switch shorts this to the ground wire, which is also at the original source point (effectively a 2km round trip) using telephone cable.

    image

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to mcb1

    Thanks Mark! That is exactly what I was looking for. My intention was to use an 8 channel optocoupler relay board, so the relays themselves can be powered remotely. If you are currently running 2km of wire, mine should be fine as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to Former Member

    01221

    There are some things to watch for on commercial opto relay boards.

     

    They are really designed for 12v trigger, and some may not function using 5v switching.

     

    It is relatively simple to either bridge the on board LED (not the best) or add a lower value resistor across the series resistor (usually a 1k).

    Terry King has the details on his site.

    Opto-Isolated 8 Channel Relay Board(Price reduced again)

     

    BTW the varistor is across the switch contact to prevent lightning from causing any issues if the switch is open.

    During the off season we tend to unplug the board, but you might want to consider lightning as it can cause one 'ground' to rise above another 'ground'.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 9 years ago in reply to Former Member

    01221

    There are some things to watch for on commercial opto relay boards.

     

    They are really designed for 12v trigger, and some may not function using 5v switching.

     

    It is relatively simple to either bridge the on board LED (not the best) or add a lower value resistor across the series resistor (usually a 1k).

    Terry King has the details on his site.

    Opto-Isolated 8 Channel Relay Board(Price reduced again)

     

    BTW the varistor is across the switch contact to prevent lightning from causing any issues if the switch is open.

    During the off season we tend to unplug the board, but you might want to consider lightning as it can cause one 'ground' to rise above another 'ground'.

     

    Mark