Arduino Forum 256 x 12 RAM
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
  • State Suggested Answer
  • Replies 13 replies
  • Answers 4 answers
  • Subscribers 393 subscribers
  • Views 1301 views
  • Users 0 members are here
  • lodgic
  • computers
  • rom
Related

256 x 12 RAM

timswift
timswift over 9 years ago

Hi

I have been designing a 4 bit computer with a 256 word program space.  But for the goto (skip to) command to work I need a 8 bit address

with a 4 bit op code.  So a 256 x 12 RAM would be needed but I cant seem to find any available.

Would a 256 x 16 work?

 

Thanks

 

Tim

  • Sign in to reply
  • Cancel

Top Replies

  • timswift
    timswift over 9 years ago in reply to johnbeetem +2
    I have finished the control logic's ruff design. I also changed the commands their are only 12 now (the ALU functions are on the same command). And the ALU has the highest chip count so far but the design…
  • dougw
    dougw over 9 years ago in reply to timswift +1 suggested
    SRAM is volatile unless it has a battery backup. Presumably you need non-volatile memory with a parallel interface. It will be tough to get modern memory chips this small so you could end up with unused…
  • DAB
    DAB over 9 years ago in reply to timswift +1
    Yes, RAM or ROM, all you need to do is provide an address bus to select the byte and a clock to latch the data inside the device to the pins on your MCU to read. In my bit slice days, we did a lot of this…
Parents
  • DAB
    0 DAB over 9 years ago

    Yes, as long as you make sure the unused data bits are properly terminated so that you do not get any ESD issues.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • DAB
    0 DAB over 9 years ago

    Yes, as long as you make sure the unused data bits are properly terminated so that you do not get any ESD issues.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • timswift
    0 timswift over 9 years ago in reply to DAB

    Sorry I wrote ROM not SRAM (it cant be volatile).

     

    Could I combine two  256 x 8 SRAM's and get a 256 x 16?

     

    Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to timswift

    I think you have this:

         So data would be only 12 bits not 16.

    It could be also:

         1st ROM uses bits 0-3 and 4-7 or each 4 bit word PLUS

         2nd ROM uses bits 0-3 and 4-7 are don't care.

    Take your pick,

     

    Clem

     

    PS. you may want to look at Intel 4004 for guidance: https://en.wikipedia.org/wiki/Intel_4004

    and history where the designer Federico Faggin was disowned by Intel The Intel 4004 Home

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 9 years ago in reply to timswift

    SRAM is volatile unless it has a battery backup.

    Presumably you need non-volatile memory with a parallel interface.

    It will be tough to get modern memory chips this small so you could end up with unused memory space.

    As mentioned two 8 bit memories will work for a 12 bit requirement, just 4 bits will be unused.

    You could use a dual-port static RAM with battery-backup which would allow an external device to load or monitor the memory.

    Or you could use FRAM - you would need 2 chips like FM16W08-SGTR - this is non-volatile RAM with a parallel interface.

    For your application:

    • connect 8 address lines in parallel and ground the unused address lines
    • use 4 bits of one FRAM to store op-codes, connect the 4 unused data pins to 100K pull-down resistors
    • The second FRAM would store 8-bit addresses.
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • DAB
    0 DAB over 9 years ago in reply to timswift

    Yes, RAM or ROM, all you need to do is provide an address bus to select the byte and a clock to latch the data inside the device to the pins on your MCU to read.

     

    In my bit slice days, we did a lot of this type of circuits to get odd data segments.

     

    DAB